D3349896_02

Downloading Clipsal C-Bus Manager Mobile Application

Prerequisite for Android device

  • Requires Android 10.0 or higher.

  • Search term: Clipsal C-Bus manager mobile app.


Prerequisite for iOS device

  • Requires iOS 13.4 or higher.

  • Search term: Clipsal C-Bus manager mobile app.


Follow the below steps to download the Clipsal C-Bus manager mobile app:

  1. Install the Clipsal C-Bus manager mobile app on a mobile phone to commission and work with the C-Bus Controller and devices.

  2. Tap the app icon and launch the application on your mobile phone.

    NOTE: The Clipsal C-Bus Manager mobile app uses your device’s browser for user authentication processes such as login, new user registration, and password reset. The app supports only Safari, Chrome, and Microsoft Edge. Make sure that one of these browsers is set as your default browser on your mobile device settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?