DUG_Inverter and Storage_WH-03

About the Document

Document Scope

This document provides comprehensive guidance on the Schneider Inverter and Boost system, detailing its features, installation procedures, configuration options, and commissioning steps using the eSetup and Wiser Home apps. Users can track solar production, battery status, and grid interaction through the Wiser Home interface. The document also includes instructions for updating firmware, accessing device insights, and managing user data. It supports flexible system setups and offers tools for optimizing energy consumption and cost efficiency.

Validity Note

The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information.

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, ARC FLASH, AND FIRE
  • This equipment must only be installed, configured, and serviced by qualified electrical personnel.
  • Qualified electrical personnel must apply appropriate personal protective equipment (PPE), follow safe electrical work practices, and adhere to all applicable local and national electrical codes.
  • Do not disassemble, alter the product, or modify the software code without authorization.
  • Never operate energized with covers removed
  • Energized from multiple sources. Before working with cables, identify all sources, deenergize, lock-out, and tag-out and wait five minutes for circuits to discharge.
  • Always use a properly rated voltage sensing device to confirm that all circuits are deenergized.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF ELECTRIC SHOCK AND FIRE
  • Before powering on equipment, verify that all wiring is in good condition and that wire is not undersized. Do not operate the inverter with damaged or substandard wiring.
  • Do not operate the inverter and battery if it has been damaged in any way.
  • Do not disassemble the battery except where noted for connecting wiring and cabling.
  • Use only the accessories that are recommended by the manufacturer.
  • Do not alter, damage, or obscure the markings and nameplates on the device.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

WARNING
HAZARD DUE TO UNINTENDED USE
The inverter and battery is not intended for use in connection with life support systems or other medical equipment or devices. They can only be used in grid-interconnected, and integrated PV systems. It is not suitable for any other application areas.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

WARNING
RISK OF ELECTRIC SHOCK AND EQUIPMENT DAMAGE
  • Keep inverter cables at least 30 mm away from any heat source. The use of inverter cables in a high temperature environment may cause aging and damage to the insulation layer.
  • Similar cables should be tied together, and different types of cables should be arranged at least 30 mm apart. Avoid cable cross-over.
  • Tighten the cables to the torque specifications in the Schneider Inverter Installation and Operation Guide.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Use cybersecurity best practices to help prevent unauthorized access to the system software.
Failure to follow these instructions can result in equipment damage.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Environmental Data

Find and download comprehensive environmental data about your products, including RoHS compliance and REACH declarations as well as Product Environmental Profile (PEP), End-of-Life instructions (EOLI) and much more.


https://www.se.com/myschneider

General information about Schneider Environmental Data Program

Click the link below to read about Schneider Electric’s Environmental Data Program.


https://www.se.com/ww/en/about-us/sustainability/environmental-data-program/

Declaration of Conformity

Hereby, Schneider Electric Industries SAS, declares that this product is in compliance with the essential requirements and other relevant provisions of RADIO EQUIPMENT DIRECTIVE 2014/53/EU.

Declaration of conformity can be downloaded on:

Available Languages of the Document

The document is available in these languages:

  • English

  • German

  • Spanish

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

  • Zigbee® is a registered trademark of the Connectivity Standards Alliance.
  • Apple® and App Store® are brand names or registered trademarks of Apple Inc.
  • Google Play™ Store and Android™ are brand names or registered trademarks of Google Inc.
  • Wi-Fi® is a registered trademark of Wi-Fi Alliance®.
  • Wiser™ is a trademark and the property of Schneider Electric, its subsidiaries and affiliated companies.
  • QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries

Other brands and registered trademarks are the property of their respective owners.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?