DUG_Inverter and Storage_WH-03

Firmware Automatic Update

Select the devices to be automatically updated to the latest firmware. This will allow the devices to update to the latest firmware with the newest features when it becomes available.
  1. On the Control tab, tap All > Inverter > Device settings.
  2. Enable the toggle switch to enable auto firmware update.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?