DUG_Inverter and Storage_WH-03

Using the device

After pairing the inverter with the Wiser Home app, you will be able to see the Inverter, Battery, and Solar Panel in Control tab under Energy Center.
NOTE:
  • If the 'Solar & Storage' installation does not include a battery but has a Grid measuring device linked to the inverter, then during commissioning, the system will only display the Solar Panel component of the inverter in the Wiser system and will not display the Grid equipment.

  • If the battery is installed later, you will need to recommission the Solar & Storage system and include the battery.

Refer to Commissioning via Wiser Home. The commissioning process should be performed by authorized or professional installers.

Inverter

In Wiser Home app, Control tab, tap on Inverter to access the Device Control Screen.

Tap Device Details to view the Firmware Version and Serial Number of the Inverter.
Tap Name in device details page to rename the inverter according to your preference.

Battery

In Wiser Home app, Control tab, tap on Battery to access the Device Control Screen.

In the Device Control Screen, you can see the following:

  • Instant available power (kW) (A)

  • Current state of battery (B)

  • Current state of charge (C)

  • History of power storage (D)

  • Device details (E)

Tap Device Details to view including the Name (F) and Serial Number (G) of the battery.
Tap Name in device details page to rename the battery according to your preference.

Solar Panel

In Wiser Home app, Control tab, tap on Solar Panel to access the Device Control Screen.

In the Device Control Screen, you can see the following:

  • Instant power generation (kW) (A)

  • Current state of solar panel (B)

  • History (C)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?