DUG_Inverter and Storage_WH-03

Resetting PIN using eSetup app

If you forgot your PIN, tap Reset PIN and then tap Continue on the popup message.

  1. Enter the code Manually: manually enter the serial number located on the dongle.

  2. Scan Barcode: scan the barcode located on the side of the inverter. Make sure to enable camera permission in the app settings.

Create the New PIN to continue the commissioning process.

Refer to Troubleshooting, if you are unable to connect with the dongle.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?