DUG_Inverter and Storage_WH-03

About Schneider Inverter and Boost

Schneider Inverter

Schneider Inverter is a one and three-phase high-performance inverter with a high conversion efficiency that powers your home and saves on your electricity bills. The inverter supports a broad range of solar array sizes and comes with integrated MPPT (Maximum Power Point Tracking) optimizers, ensuring maximum power output. It can be upgraded with Schneider Boost batteries to maximize self consumption

  • Advanced DSP (Digital Signal Processing) control technology

  • Integrated MPPT optimizers for maximum power output.

  • Supports wider MPPT voltage range.

  • Low conversion losses due to DC coupling.

  • LED status indication

  • IP65 protection, can be installed in both indoor and outdoor environments

  • Scalable in system capacity by connecting multiple battery modules per inverter.

  • New Wi-Fi data monitoring technology

  • Flexible installation - indoor or outdoor.

  • Compact design that requires minimum space.

  • Advanced safety features, including emergency power shutdown and embedded Residual Current Monitoring Unit.

  • Fast commissioning through the Wiser Home App and eSetup app.

  • Real-time energy monitoring from anywhere, with the easy-to-use Wiser Home App for Monitoring or HEMSLogic App for Sectorcoupling.

Schneider Boost

The Schneider Boost storage system includes a Battery Controller (BATPMEU2) and several battery modules (BATB3KEU3), which can store and release electrical energy according to the requirements of the inverter management system.

  • Battery charging: The Battery Controller is connected to the inverter's battery terminals (BAT+, BAT-). Under the control of the inverter, the battery is charged and the excess photovoltaic energy is stored in the battery
  • Battery discharge: When the photovoltaic energy is not enough to power the loads, the system controls the battery to power the loads: the energy stored by the battery is output to the loads through the inverter.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.