Schneider Inverter and Boost
Schneider Inverter

Single Phase Inverter: HY5K1EU1, HY6K1EU1, HY8K1EU1
Three Phase Inverter: HY8K3EU1, HY10K3EU1, HY14K3EU1
Schneider Boost

Battery Controller: BATPMEU2
Battery Module: BATB3KEU3

Single Phase Inverter: HY5K1EU1, HY6K1EU1, HY8K1EU1
Three Phase Inverter: HY8K3EU1, HY10K3EU1, HY14K3EU1
Schneider Boost

Battery Controller: BATPMEU2
Battery Module: BATB3KEU3
- About Schneider Inverter and Boost
- Solar Inverter and Boost configurationYou can configure the Solar Inverter and Boost system according to power utilization in your home.
- Installation guides
- Installer Process
- Pairing the device to Wiser systemThe Schneider Inverter can be paired with the Wiser Home app to monitor the power flow.
- Using the deviceAfter pairing the inverter with the Wiser Home app, you will be able to see the Inverter, Battery, and Solar Panel in Control tab under Energy Center.
- TariffSet tariff in the Wiser Home app to view energy costs and billing information.
- Wiser Home AIUse the Wiser Home app, to view device control and schedules.
- Checking device consumptionUsing the Wiser Home app, you can monitor the live, history of Grid, Solar and individual loads as well as statistical analysis of energy consumption of all the loads installed with Energy meter
- Delete the personal data
- Firmware Automatic UpdateSelect the devices to be automatically updated to the latest firmware. This will allow the devices to update to the latest firmware with the newest features when it becomes available.
- LED indications
- Maintenance and troubleshooting
- Technical specifications
- Compliance with local regulations