Live
- On the bottom navigation bar, tap
.
- Tap Live.
- Grid import: The live graph shows the real-time electricity
pricing throughout the day. You can interact with the graph to
see when the most expensive times are based on your tariff.
NOTE: This graph is displayed only if you set your tariff to Peak/Off-Peak or Dynamic. Refer to Setting Tariff
- Grid import and export (Applicable for Grid with On Grid
solar system): The grid consumption with loads is represented
in blue and the excess energy of solar production sold is represented
in green.
- Grid, Solar and Battery
-
Grid: Represented in blue.
-
Solar (PV): Represented in green.
-
Battery: Represented in grey
Scroll down to view the graph.
NOTE: Ensure to pair the Schneider Inverter and Boost in daylight to have the PV equipment (Green) to be available in Live.-
Consumption total: It shows the total energy consumption in kWh.
-
Solar production: It shows the energy produced by the solar system in kWh.
-
Self-sufficiency: It shows the percentage of energy produced by the solar system that is consumed by the household.
-
% of production used: It shows the percentage of solar energy that is used.
-
- Grid import: The live graph shows the real-time electricity
pricing throughout the day. You can interact with the graph to
see when the most expensive times are based on your tariff.