DUG_Energy Monitoring Device-01

Adding devices to favourites

To add favourites:
  1. On the Dashboard (A) page, tap Click here (B) / Add + (C).
    The Manage Favourites page appears.
  2. Select a device from the list (D).
    NOTE: You can select multiple devices as favourites.
  3. Tap Done (E).
    Now, you can see the devices on the Dashboard page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?