DUG_Energy Monitoring Device-01

Load Details

Loads are the channels connected to the device apart from the main incomer or grid.
  1. On the home screen, tap Devices.
  2. Select the device under Energy Management.
  3. Select any one of the load channel (A).
    Now Load tab will be open.
    You will find following two tabs under Load:

Live

  1. Tap Load (A) > Live (B).
  2. To know the live power consumption see Power Now (C).
  3. You can find today’s, this week’s, and this month’s consumption with the monetary value (D).

Metrics

  1. Tap Load (A) > Metrics (B).
You can see the details about the energy parameters in this tab.

Devices

  1. Tap Devices.
    You can see the devices linked with the load channel.
  2. To Link a new device:
    1. Tap Link Devices (A).
    2. Tap Select Connected device (B) and select the device you want from the drop down.
    3. Tap Add (C) > OK.
  3. To remove an existing linked device:
    1. On the top right corner, tap icon.
    2. On the side of the device, tap icon > OK.
  4. To turn on a device tap available on the side of the device.
  5. To turn off a device tap available on the side of the device.

Timeline

Refer Timeline for more information.

    Settings

    1. Tap Devices.
    2. Select the device under Energy Management.
    3. Select the Load channel.
    4. Tap Settings.
    You will find following tabs:

    Connected Loads

    You can find and add connected loads from this option.
    1. Tap Devices.
    2. Select the device under Energy Management.
    3. Select the Load channel.
    4. Tap Settings. > Connected Loads > Add Connected Load (A).
    5. Select load from the drop-down (B).
      Note: If you want to add a new load, select Others (C) and enter new load in in Select Load field.
    6. Tap Add.

    Change Room

    You can select or add new room from this option.
    1. Tap Devices.
    2. Select the device under Energy Management.
    3. Select the Load () channel.
    4. Tap Settings. > Change Room.
    5. Select the room from the list.
      Note: To add a new room name:
      1. Tap .

      2. Enter room name.

      3. Tap Add Room.

    QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

    Was this helpful?