DUG_Energy Monitoring Device-01

Budgeting

Budgeting allows you to set your budget on monthly power consumptions and create alert once you reach certain percentage of that budget.
  1. Tap Devices.
  2. Select the device under Energy Management.
  3. Select the Grid () channel.
  4. Tap Settings > Budgeting.
  5. Tap Set budget (A).
  6. Tap against each month field to update Set monthly budget (B) in kWh.
  7. Drag the slider button to set the Alert 1 (C) and Alert 2 (D) for monthly budget.
    NOTE: Alert 1 value should always be less then Alert 2value.
    NOTE: Weekly Budget and Daily Budget are calculated pro rata based onMonthly Budget.
  8. Tap Save (E) > OK.
  9. To enable Push Notifications, tap button.
    The app will send you notification of alerts.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?