DUG_Energy Monitoring Device-01

Power Alerts

You can create Power Alerts based on the selected channel (Maximum four alerts). These alerts will be used as a part of trigger action.
  1. Tap Devices.
  2. Select the device under Energy Management.
  3. Select the channel for which you need to set the alert.
  4. Tap Settings (A) > Power Alerts (B).
    Note: You will get option to set maximum of four alerts based on channel selected.
  5. Select any of the Alert to update following fields (C):
    1. Alert Name: Tap to add the name of alert.
    2. When: Select Greater Than or Less Than from the drop-down.
    3. Select Value: Tap to add the value.
    4. Units: Select the unit from drop-down.
  6. Tap Save (D) to save the alert.
    NOTE: To enable or disable Power Alerts from the device, use the toggle switch (E).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?