DUG_Energy Monitoring Device-01

Grid Details

You can see the detailed information about grid in the Wiser app.
  1. Tap Devices.
  2. Select the device under Energy Management.
  3. Select the channel which is selected as grid (A).
Now Grid tab will be open.

Live

  1. Tap Grid (A) > Live (B).
  2. To know the live power consumption see Power Now (C).
  3. You can find today’s, this week’s, and this month’s consumption with the monetary value (D).

Budget

  1. Tap Grid (A) > Budget (B).
    1. To see day wise budget, tap Day (C) > > select the date > OK.
    2. To see week wise budget, tap Week (D) > > select the week > OK.
    3. To see month wise budget, tap Month (E) > > select the month > OK.
  • You can see the daily, weekly, monthly budget details.

  • you can see the allocated budget, how much you have consumed till now, how much CO2 saved, what is the alert values (F).

Metrics

  1. Tap Grid (A) > Metrics (B).
You can see the details about the energy parameters in this tab.

Devices

You need to have smart devices linked to the incomer to use this feature.
  1. Tap Devices (A).
    You can see the loads associated with the main incomer.
  2. To view associated smart devices (C), tap the drop-down list (B) of the required load.
    You can turn them on () or off () as needed.

Timeline

Refer Timeline for more information.

    Settings

    Refer Settings for more information.

    QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

    Was this helpful?