DUG_Energy Monitoring Device-01

Removing the device

Using the Wiser app you can remove a device from the device list.
To remove the device:
  1. On the Devices page, tap Devices.
  2. On the top right corner of the screen, tap .
    The Edit Device List page appears.
  3. Tap the remove button (A) which is next to the device name.
    The pop-up message will appear to confirm the delete action.
  4. Tap Delete (B).
  5. Tap Delete Energy Meter (C) and then select Ok.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to resetting the device.
  6. Alternatively, you can also unpair the device manually by pressing the push Reset button 14 times.
    NOTE: When you manually unpair the device, you can still see the device name in the Wiser App.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?