DUG_Energy Monitoring Device-01

Setting Device Alerts

Set your voltage limits to get notified during abnormal voltage fluctuations.
  1. Tap Settings (A) > Device Alerts..
  2. Tap to enter the Voltage Hysteresis Value (B) and Current Hysteresis value (C).
  3. Tap to enter the Power Cutoff Value (D).
  4. Drag the slider button to set the Lower Limit of the Voltage (E).
  5. Drag the slider button to set the Upper Limit of the Voltage (F).
  6. Tap Save (G) > OK.
  7. To enable Push Notifications, tap button.
    The app will send you notification of alerts.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?