DUG_Energy Monitoring Device-01

Current Alerts

Set your current limit to get notified during abnormal current fluctuation.
  1. Tap Devices.
  2. Select the device under Energy Management.
  3. Select the channel for which you need to set the limit.
  4. Tap Settings (A) > Current Alerts.
  5. Drag the slider button to set the Current limit (B).
  6. To enable Push Notifications tap button (C).
    The app will send you notification of alerts.
  7. Tap Save (D) > OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?