DUG_Energy Monitoring Device-01

Power Factor Alerts

Get notified when the power factor is below the set value.
  1. Tap Devices.
  2. Select the device under Energy Management.
  3. Select the channel for which you need to set the alerts.
  4. Tap Settings (A) > Power factor Alerts.
  5. To enable Push Notifications, tap button (B).
    • The alert screen will come.

    • You can set up to three power factor alerts for the device.

  6. Drag the slider buttons to set the alerts (C).
    NOTE: The alerts should be in following order:

    Alert 1 value should be greater then Alert 2 value.

    Alert 2 value should be greater then Alert 3 value.

  7. Tap Save > OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.