DUG_Energy Monitoring Device-01

Changing the Wi-Fi access point

To change the device Wi-Fi:
  1. On the Devices page, select the energy monitoring device which you wish to change the Wi-Fi.
  2. On the top-right corner of the screen, tap Settings (A).
  3. If Device Status is Online:
    1. Tap Change Access Point (B).
      A pop up will appear, asking for password of Wiser app.
    2. Tap Please enter password and enter the Wiser app password and Tap Confirm.
    3. Select your preferred Wi-Fi network and enter the password in Wi-Fi Password field and tap Connect.
  4. If Device Status is Offline:
    1. Tap Change Access Point.
      A pop up will appear, asking for password of Wiser app.
    2. Tap Please enter passwordfield and enter the Wiser app password and Tap Confirm.
      This will initiate the pairing mode in the Wiser app.
    3. Follow Pairing the device for further process.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?