DUG_Energy Monitoring Device-01

Installing the device

Refer to the installation instruction supplied with this product.

Instruction manual link:

NOTE: It is recommended to install the patch antenna within range of the Wi-Fi router for best results. This provides a good network strength and helps to prevent online/offline issues, which might result in corrupting data.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?