DUG_Energy Monitoring Device-01

Resetting the device

You can reset the device to factory default manually.

Short-press the push button 14 times.The LED blinks pink for 10 s.

NOTE: After reset, the device is ready for pairing.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?