Assign Domains
To assign a domain to a particular field, it must be done by adding the domain attribute to a column tag in DatabaseSchemaConfig.xml. For example:
<Column Name="CRITICAL" Caption="Critical" Domain="CRITICAL_TYPE" Represents="CriticalCustomer"/>
Virtual Domains
Responder creates some domains that are NOT defined in DatabaseSchemaConfig.xml. To use these domains, they must be assigned to a field (or column) in a table. Below are descriptions of the virtual domains automatically created by Responder.
|
Domain |
Description |
|---|---|
|
CREW_MEMBER |
This domain contains a list of members in the RX_CREW_MEMBERS table. |
|
FACILITY_TYPE |
This domain contains a list of all feature classes in the geodatabase. In the DatabaseSchemaConfig.xml file installed with Responder, this domain is assigned to all FCID fields (e.g., DEVICE_FCID, FCID, INCIDENT_DEVICE_FCID). |
|
REGION |
This domain contains a list of regions in the RX_REGIONS table. |
|
USERS |
This domain contains a list of users in the RX_USERS table. |
Calculated Fields
A calculated field uses a domain value selected by the user to perform a calculation and present the result. For example, a user may select a value of 1 hour from the Time Restored Est. field. The Time Restored Est. field uses this value (1 hour) to calculate the estimated time of restoration.
In the case of a calculated field, the domain is not assigned to the field in DatabaseSchemaConfig.xml. However, the domain must be defined in DatabaseSchemaConfig.xml.
Below is a list of calculated fields in Responder:
|
Field |
Domain |
Calculation |
|---|---|---|
|
Time Restored Est. |
INCIDENT_DURATION |
The user-selected domain value (e.g., 1 hr) is added to the current time for an estimated time of restoration. You may modify the INCIDENT_DURATION domain. The field will use the custom values in its calculation. |