RX_SW_OR_FEATURES_HISTORY
|
Field Name |
Description |
|---|---|
|
SW_OR_FEATURES_ID |
The unique ID assigned to the switching order feature. |
|
OID |
Object ID of the feature that was operated upon. |
|
FCID |
Feature class ID of the feature that was operated upon. |
|
SUBID |
The unique ID of each segment of a complex edge. |
|
X |
The x-coordinate of the incident device. |
|
Y |
The y-coordinate of the incident device. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
FACILITY_ID |
The Facility ID of the incident device as defined in the geodatabase. |
|
REGION |
The region in which the switching order feature is located. This field uses the REGION domain. |
|
SUBSTATION |
The substation that feeds the incident device. |
|
COMMENTS |
Notes from the operator or dispatcher. |
|
ENABLED |
Not used. |
|
SUBTYPE |
The subtype of the device. |
|
FEEDER_ID |
The ID of the feeder. |
|
PHASE_DESIGNATION |
The phase designation of the device. |
|
OPERATING_VOLTAGE |
The operating voltage of the device. |
|
NAME |
The name assigned to the device. |
|
CHANGE_DATE |
The date an operation was performed on the incident record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |
|
SW_ORDER_REQUEST_ID |
The unique ID assigned to the switching order request. |
|
AFFECTS_ENERGIZATION |
Indicates whether the feature participates in the geometric network (electric device) or not (location feature). |