RX_CREW_ASSIGNMENTS_ARCHIVE
|
Field Name |
Description |
|---|---|
|
ASSIGNMENT_ID |
The unique identifier assigned to each crew assignment. This field corresponds with the ID field in the RX_CREW_ASSIGNMENTS table. |
|
INCIDENT_ID |
The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table. |
|
CREW_ID |
Indicates the ID for the crew that has been assigned to the incident. This field corresponds to the ID field in the RX_CREWS table. |
|
STATUS |
Indicates the status of the crew. This field uses the STATUS domain. |
|
TIME ASSIGNED |
The time the crew was assigned to the incident. |
|
IS_LEAD_CREW |
Indicates whether the crew is the lead crew. This field uses the IS_LEAD_CREW domain. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
|
USER_UPDATED_ARCH |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
TIME_STATUS_CHANGED |
This is the time that a crew's status was changed (e.g., from Dispatched to Working) after it was modified by a dispatcher. |