RX_LOADPOINTS
|
Field Name |
Description |
|---|---|
|
DEVICE_OID |
The object ID of the incident device affecting the loadpoint (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
DEVICE_FCID |
The feature class ID of the incident device affecting the loadpoint (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
INCIDENT_ID |
The ID associated with the incident associated with the loadpoint. This field acts as a foreign key to the RX_INCIDENTS table. |
|
TIME_OUTAGE |
The time the outage occurred. |
|
TIME_RESTORED |
The time power is actually restored. |
|
CUSTOMER_COUNT |
Indicates the number of customers affected by the incident. |
|
CRITICAL_CUSTOMER_COUNT |
Indicates the number of critical customers affected by the incident. |
|
PRIORITY_CUSTOMER_COUNT |
Indicates the number of priority customers affected by the incident. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
INCIDENT_DEVICE_OID |
The object ID of the device to which the incident is associated (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
INCIDENT_DEVICE_FCID |
The feature class ID of the device to which the incident is associated (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
CUSTOMER_ACCOUNT |
The customer's account number. |