RX_JUMPER_STEPS_ARCHIVE
|
Field Name |
Description |
|
JUMPER_STEP_ID |
The ID associated with the Jumper. |
|
OPERATION_ID |
The ID field from RX_OPERATIONS (foreign key). |
|
TRACE_WEIGHT |
Field containing information used by Feeder manager to utilize the Jumper when tracing the network. |
|
EDGE1_FCID |
Feature class ID of the first initial conductor clicked to place the Jumper. |
|
EDGE1_OID |
The object ID of the first initial conductor clicked to place the Jumper. This field links to the OID field in your geodatabase. |
|
EDGE1_SUBID |
The subnetwork ID of the Edge that represents the initial snap point of a Jumper. |
|
EDGE2_FCID |
Feature class ID of the second and final conductor clicked to place the Jumper. |
|
EDGE2_OID |
The object ID of the second and final conductor clicked to place the Jumper. This field links to the OID field in your geodatabase. |
|
EDGE2_SUBID |
The subnetwork ID of the Edge that represents the terminating snap point of a Jumper. |
|
DISPATCHED_BY_NAME |
The name of the dispatcher who executed the Jumper. |
|
Points |
This field represents all the points on the map a user clicked when creating a Jumper. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
|
JUMPER_GUID |
The GUID assigned to the Jumper. |
|
STEP_TYPE |
Field that differentiates between steps that Place or Remove Jumpers. |
|
JUMPER_NAME |
The name assigned to your Jumper. |