RX_LOADPOINTS_HISTORY
|
Field Name |
Description |
|---|---|
|
LOADPOINT_ID |
The unique identifier assigned to the loadpoint. This field corresponds to the ID field in the RX_LOADPOINTS table. |
|
DEVICE_OID |
The object ID of the incident device affecting the loadpoint (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
DEVICE_FCID |
The feature class ID of the incident device affecting the loadpoint (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
INCIDENT_ID |
The ID associated with the incident associated with the loadpoint. This field corresponds with the ID field in the RX_INCIDENTS table. |
|
TIME_OUTAGE |
The time the outage occurred. |
|
TIME_RESTORED |
The time power is actually restored. |
|
CUSTOMER_COUNT |
Indicates the number of customers affected by the incident. |
|
CRITICAL_CUSTOMER_COUNT |
Indicates the number of critical customers affected by the incident. |
|
USER_CREATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record. |
|
USER_UPDATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
CHANGE_DATE |
The date an operation was performed on the incident record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |
|
INCIDENT_DEVICE_OID |
The object ID of the device to which the incident is associated (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
INCIDENT_DEVICE_FCID |
The feature class ID of the device to which the incident is associated (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
PRIORITY_CUSTOMER_COUNT |
Indicates the number of priority customers affected by the incident. |
|
CUSTOMER_ACCOUNT |
The customer's account number. |