RX_SW_OR_REQUESTS_HISTORY
|
Field Name |
Description |
|---|---|
|
SW_OR_REQUESTS_ID |
The unique ID assigned to the switching order request. |
|
TOTAL_CUSTOMERS_COUNT |
The total number of customers affected by the switching order request. |
|
CRITICAL_CUSTOMERS_COUNT |
The number of critical customers affected by the switching order request. |
|
PRIORITY_CUSTOMERS_COUNT |
The number of priority customers affected by the switching order request. |
|
NAME |
The name associated with the switching order request. |
|
PHONE_NUMBER |
The phone number associated with the switching order request. |
|
FEEDER_ID |
The ID of the feeder. |
|
REGION |
The region in which the switching order feature is located. This field uses the REGION domain. |
|
SHORT_DESCRIPTION |
The short description provided with the switching order request. |
|
PLANNED_BEGIN_TIME |
The planned time for the work in the request to begin. |
|
PLANNED_END_TIME |
The planned time for the work in the request to be completed. |
|
REASON |
The reason provided for the switching order request. |
|
STATUS |
The status of the switching order request. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
REQUEST_REFERENCE |
The reference number assigned to the request. |
|
SWITCHING_ORDER_ID |
The unique ID that identifies the switching order to which the request has been assigned. |
|
CHANGE_DATE |
The date an operation was performed on the incident record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |