Submit Rules
Responder uses submit rules to control the logical flow of the application. For example, a user is required to enter a time and user name when restoring an electric device. A submit rule enforces this requirement by keeping the OK button disabled until the required information is supplied.
While most submit rules are necessary, Responder does provide several submit rules that may be enabled or disabled. You may enable/disable ONLY the submit rules listed below. Do not disable any other submit rules. The following rules may be enabled or disabled in the SubmitRulesConfig.xml file which is installed here: Program Files (x86)\Miner and Miner\Responder\Server\. To enable a submit rule, simply remove the characters that comment it out of the XML (<!-- and -->). To disable, comment it out.
|
Submit Rule |
Description |
Default Setting |
OK to Modify? |
|---|---|---|---|
|
ArchiveIncidentHistoryRule |
This rule is enabled by default and has two properties:
|
ArchiveCanceledIncidents is set to False DeleteHistory is set to True. |
Yes |
|
ExecuteSwitchingOperation |
Populates Field Remarks field of an incident with comment from switching order operation. When commented out (default) the behavior is to store and archive this field value as a switch order step comment. |
Disabled |
Yes |
|
PopulateUserCreated |
Populates the User_Created field in all tables. |
Enabled |
Yes |
|
PopulateUserUpdated |
Populates the User_Updated field in all tables. |
Enabled |
Yes |
|
PreventUpdatesToMobileCrewTasks |
Prevents a dispatcher from editing an incident that has been sent to a crew in the field.
IMPORTANT: If you disable
this submit rule, you MUST establish a work or business process that
prevents conflicts. Disabling this rule makes it possible to create
conflicts between the field and the Enterprise.
*We recommend against disabling this submit rule. |
Enabled |
Yes *Read Important note in Description column first |
|
RemoveTagsPlacedViaSwitchingOrderWhenCanceled |
Removes tags that have been placed as part of a switching order when that switching order is cancelled. |
Enabled |
Yes |
|
SecureDownstreamHazards |
When all affected phases are open, this submit rule identifies downstream hazards on the open phases and designates them as clear or safe to work on. |
Disabled |
Yes |
|
UpdateHazardWhenCrewWorking |
Secures a hazard when the crew is working. |
Disabled |
Yes |
|
UpdateLeadCrewAssignmentAdded |
Updates the Lead Crew field based on crews added. |
Enabled |
Yes |
|
UpdateLeadCrewAssignmentModified |
Updates the Lead Crew field based on crews edited. |
Enabled |
Yes |
|
UpdateLeadCrewAssignmentDeleted |
Updates the Lead Crew field based on crews deleted. |
Enabled |
Yes |
|
ValidateCrewAssignability |
Prevents a crew from being dispatched to multiple incidents at the same time. The crew must complete an incident before being dispatched to another. It can have a Dispatched or Working status on only one incident at a time. Disable this rule to be able to dispatch a single crew to multiple incidents. |
Enabled |
Yes |
|
ValidateIncidentDeviceTimeOpChange |
This rule determines the circumstances under which the Time of Operation field may be edited. The Time of Operation field may be edited only in the following situations:
To change this rule (disable it or modify the parameter), it must be modified in SubmitRulesConfig.xml and ExplorerRulesConfig.xml. IMPORTANT: If this submit rule is disabled, there are
particular scenarios with backdating that may cause issues with load
point outage and restoration times.
|
Enabled |
Yes *Read Important note in Description column first |
|
ValidateIncidentDeviceTimeOpOnStatusChange |
This rule impacts the Time of Operation for incident devices that are undergoing a phase change or devices that are added to an existing incident. This rule prevents these devices from having a Time of Operation that is earlier than the Time of Operation for any existing device on that incident. This rule has a parameter called ApplyToConfirmedOnly. When set to True, this rule applies only to confirmed incidents. When set to False, this rule applies to all incidents. Default=True. To change this rule (disable it or modify the parameter), it must be modified in SubmitRulesConfig.xml and ExplorerRulesConfig.xml. IMPORTANT: If this submit rule is disabled, there are
particular scenarios with backdating that may cause issues with load
point outage and restoration times.
|
Enabled |
Yes *Read Important note in Description column first |
|
VerifyTagsAllowIncidentCancelation |
Throws an error if cancelling or deleting an incident device will cause the device will violate a tag as it returns to a normal state. |
Enabled |
Yes |
|
VTextOutageAlert |
With proper configuration, this submit rule enables sending a text message based on configurable parameters. TIP: In addition to enabling this rule, edit the vtext.txt
file which is installed here: Program Files (x86)\Miner and Miner\Responder\Server\
with the appropriate sender, receiver, and subject information. |
Disabled |
Yes |