Prediction Services Configuration
Once you have configured the Prediction Services configuration file (PredictionServices.exe.config), you must start Prediction Services. At least one Prediction Services must remain active in order for Responder's prediction engine to work.
The Count field indicates the number of Prediction Services running. If you change this value to 0 and click Apply, the Arguments field becomes enabled. Use this field to set your geodatabase server along with any arguments.
To start Prediction Services, enter the number of instances you'd like to run in the Count field and click Apply. When Prediction Services are running, you may not edit the Arguments field. The Path field always remains disabled. This field provides the path to the executable that launches Prediction Services.

Arguments
Below is a list of available arguments.
|
Argument |
Description |
|---|---|
|
-fast |
Does not initialize the geometric network on start-up. |