Remove Dashboard Values
You can remove reported information from the dashboard Analytical and Tabular sections. This is done by editing the Web.config file. By default, this file is installed here: C:\Inetpub\wwwroot\Responder.
The dashboard uses providerKeys to gather the data and controlKeys to display it. By removing the providerKey and the corresponding controlKey, you can eliminate reported data in the dashboard. You can take out only the controlKey. However, if you choose to take out only the providerKey, the display will appear broken.
- Open Web.config and look for the following bit of XML.
<add key="service.providerKeys" value="customerStatus, crewStatus, incidentStatus, wiresDownStatus, regionAreaPath, affectedLoadPoints, incidentDevicePoints, hazardPoints, callStatus, outageMonetaryStatus"/>
- The values in this XML are the providers used to populate
the data on the web application. Note that removing these can impact
other aspects of the web application. You can delete a providerKey
to stop retrieving the data. For example, delete outageMonetaryStatus
to remove the total outage cost value from the Analytical tab of the
dashboard.
Below are descriptions of the providerKeys:
-
customerStatus - Provides customer counts for the outage.
-
crewStatus - Provides counts for crews (e.g., assigned, unassigned, total crews).
-
incidentStatus - Provides incident counts (e.g., critical, total incidents).
-
wiresDownStatus - Provides hazard counts.
-
regionAreaPath - Retrieves the geometry from SDE. If you delete this, the maps will not work.
-
affectedLoadPoints - Retrieves the locations for the affected load points.
-
incidentDevicePoints - Retrieves locations of the incident devices.
-
hazardPoints - Retrieves the locations of the hazards.
-
callStatus - Provides a count of calls (e.g., processed, unprocessed, total calls).
-
outageMonetaryStatus - Provides the total cost of the outage value.
-
- Next, look for the following bit of XML in Web.config.
<add key="dashboard.grid.controlKeys" value="customerStatus, incidentStatus, crewStatus, wiresDownStatus, callStatus, outageMonetaryStatus"/>
- Remove the key that corresponds to the portion of the user
interface to remove. For example, delete outageMonetaryStatus to remove
the total outage cost value from the Analytical tab of the dashboard.
Below are descriptions of the controlKeys.
-
customerStatus - Customer Status on the Tabular tab and the Analytical tab.
-
incidentStatus - Interruption Status on the Tabular tab and the Analytical tab.
-
crewStatus - Crew Status on the Tabular tab and the Analytical tab.
-
wiresDownStatus - Hazard Status on the Tabular tab and the Analytical tab.
-
callStatus - Call Status on the Tabular tab and the Analytical tab.
-
outageMonetaryStatus - Outage Cost on the Analytical tab.
-
- Save and close Web.config.