RX_INCIDENT_DEVICES_HISTORY
|
Field Name |
Description |
|---|---|
|
INCIDENT_DEVICE_ID |
The unique identifier assigned to the incident device. This field corresponds to the ID field in the RX_INCIDENT_DEVICES table. |
|
DEVICE_OID |
The object ID of the incident device (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
DEVICE_FCID |
The feature class ID of the incident device (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
INCIDENT_ID |
The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table. |
|
TIME_OPERATION |
The time the device was opened or closed for repair. |
|
FEEDER_ID |
The Feeder ID of the incident device. |
|
SUBSTATION |
The substation that feeds the incident device. |
|
CONFIRMED |
Indicates whether the device has been confirmed out. This field uses the CONFIRMED domain. |
|
DEVICE_OPERATION |
Indicates the type of operation the device performs (Fault/Switching Operation). This field uses the DEVICE_OPERATION domain. |
|
CUSTOMER_COUNT |
Indicates the number of customers affected by the incident. |
|
CRITICAL_CUSTOMER_COUNT |
Indicates the number of critical customers affected by the incident. |
|
PRIORITY_CUSTOMER_COUNT |
Indicates the number of priority customers affected by the incident. |
|
USER_CREATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record. |
|
USER_UPDATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
CHANGE_DATE |
The date an operation was performed on the incident record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |
|
FACILITY_ID |
The Facility ID of the incident feature as defined in the geodatabase. |
|
EXPECTED_STATUS |
The expected or normal status of the device (open, closed). |
|
ACTUAL_STATUS |
The current actual status of the device (open, closed). |
|
SUBID |
The unique ID of each segment of a complex edge. |
|
X |
The x-coordinate of the incident device. |
|
Y |
The y-coordinate of the incident device. |
|
CANCEL_REASON |
Reason the device was cancelled. |
|
ADDRESS |
The address where the incident is located |
|
REMARKS |
Notes from the operator or dispatcher. |