Notify Network Change
The Notify Network Change
tool keeps the data in the geodatabase current with Responder.
When Responder loads the geometric network at start-up, it caches
the network for better performance. This tool allows you to reload
the geometric network. Refresh the version in ArcMap to view the latest
information. You should run this tool to update Responder's view of
the geometric network whenever you add, delete, or modify geometric
network features.
This tool may also be automated using the standalone executable version installed with Responder. This tool, which is run from a command prompt, is installed by default here:
C:\Program Files (x86)\Miner and Miner\Responder\Server\Tools\NetworkRefresh.exe
NetworkRefresh.exe requires you to specify the MSMQ machine necessary to communicate with Data Services. There are two ways to do this:
-
DataServices Server: Specify the name of the computer that hosts Data Services: -computer:<servername> You may also replace <servername> with "." to indicate the local machine: -computer:. In the example below, the server name is "dox."
Additional Parameters
|
-port:#### |
Use this parameter to specify a port number on the group. For example: NetworkRefresh.exe -group:172.18.226.123 -port:8005
|
|
-intf:<ip-addr> |
This parameter is necessary if you have multiple network interfaces (including virtual interfaces). Use this parameter to specify the network interface MSMQ should use. For example: NetworkRefresh.exe -group:172.18.226.123 -intf:172.18.223.321
|