RX_JUMPERS_HISTORY
|
Field Name |
Description |
|
JUMPER_ID |
The ID associated with the Jumper. |
|
JUMPER_FCID |
Feature class ID of the Jumper. |
|
JUMPER_OID |
The object ID of the Jumper. This field links to the OID field in your geodatabase. |
|
JUMPER_NAME |
The name assigned to your Jumper. |
|
TRACE_WEIGHT |
Field containing information used by Feeder manager to utilize the Jumper when tracing the network. |
|
WEIGHT_DESC |
Description of phases connected by the Jumper. |
|
EDGE_EID1 |
The edge element ID for the initial click of placing a Jumper. |
|
EDGE_EID2 |
The edge element ID for the final click of placing a Jumper. |
|
JUNCTION_EID1 |
The electrical junction to which the initial click of the Jumper is connected. |
|
JUNCTION_EID2 |
The electrical junction to which the final click of the Jumper is connected. |
|
USER_CREATED |
The name of the user who created the jumper. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the jumper. This field is populated automatically by Responder. |
|
FEEDER_ID |
All Energized feeders to which either end of a Jumper is connected. |
|
SUBSTATION |
The Substations matching the Feeders in FEEDER_ID. |
|
REGION |
The region of the initial placement of the jumper. |
|
TIME_OPERATION |
Time when the jumper was placed in the field. |
|
TIME_REMOVAL |
Time when the jumper was removed in the field. |
|
LOCATION |
A text field that can be used to better indicate jumper location. |
|
DISPATCHER |
The name of the dispatcher assigned to the jumper. This field is set on the Place Jumper form. |
|
CREW_MEMBER |
The name of the crew member assigned to the jumper. This field is set on the Place Jumper form. |
|
COMMENTS |
Comments enetered in Responder Explorer for the jumper. |
|
INCIDENT_ID |
The ID associated with the incident associated with the jumper. This field acts as a foreign key to the RX_INCIDENTS table. |
|
Points |
This field represents all the points on the map a user clicked when creating a Jumper. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
|
JUMPER_GUID |
The GUID assigned to the Jumper. |