RX_CALLS_HISTORY
|
Field Name |
Description |
|---|---|
|
CALL_ID |
The unique identifier associated with the call. This field corresponds with the ID field in the RX_CALLS table. |
|
REGION |
The region in which the call originated. This field uses the REGION domain. |
|
CRITICAL |
Indicates if the call came from a customer site that is critical. This field uses the CRITICAL_TYPE domain. |
|
HAZARD |
Indicates any hazards in the area (e.g., fire, wires down, etc.). This field uses the HAZARD domain. |
|
TROUBLE |
Indicates the problem reported by the customer (e.g., no power, flickering lights, etc.). This field uses the CALL_TROUBLE domain. |
|
DEVICE_OID |
The object ID of the device to which the customer is associated (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
DEVICE_FCID |
The feature class ID of the device to which the customer is associated (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
INCIDENT_ID |
The ID associated with the incident resulting from the call. This field corresponds with the ID field in the RX_INCIDENTS table. |
|
CUSTOMER_ACCOUNT |
The customer's account number. |
|
CALLBACK_REQUESTED |
Indicates whether the customer requested a return call. This field uses the CALLBACK_REQUESTED domain. |
|
CALLBACK_STATUS |
Indicates whether this is a Regular Callback (0) or a Power Not Restored Callback (1). This field uses the CALLBACK_STATUS domain. |
|
TIME_RECEIVED |
The time the call was received by Responder. |
|
TIME_OUTAGE |
The time the outage occurred. |
|
TIME_RESTORED |
The time the customer's power was restored. |
|
REMARKS |
Notes from the operator or dispatcher. |
|
USER_CREATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record. |
|
USER_UPDATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
CHANGE_DATE |
The date an operation was performed on the incident record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |
|
TROUBLE_AT_ACCOUNT |
Indicates whether the trouble is located at the same location as the customer's account. |
|
CAUSE |
Indicates the cause of the outage. This field uses the CAUSE domain. |
|
URGENCY |
Tells whether or not the Dispatcher marked a specific call as Urgent. |
|
ORIGINATION |
Indicates whether an incident was created by a user or by Prediction Services. |