RX_HAZARDS_HISTORY
|
Field Name |
Description |
|---|---|
|
HAZARD_ID |
The ID associated with the hazard. This field acts as a foreign key to the RX_HAZARDS table. |
|
INCIDENT_ID |
The ID associated with the incident. This field acts as a foreign key to the RX_INCIDENTS table. |
|
CALL_ID |
The unique identifier associated with the call. This field corresponds with the ID field in the RX_CALLS table. |
|
FCID |
Feature class ID of the feature associated with the tag. |
|
OID |
Object ID of the feature associated with the tag. |
|
SUBID |
The unique ID of each segment of a complex edge. |
|
FACILITY_ID |
The Facility ID of the incident device as defined in the geodatabase. |
|
X |
The x-coordinate of the incident device. |
|
Y |
The y-coordinate of the incident device. |
|
DAMAGE_TYPE |
This is the hazard type. This field uses the HAZARD_TYPE domain. |
|
STATUS |
Indicates the status of the hazard. This field uses the STATUS domain. |
|
WIRE_OWNER |
The owner of the "wires down" hazard. This field uses the HAZARD_TYPE_OWNER domain. |
|
TIME_CREATED |
The time the hazard incident was created. |
|
TIME_COMPLETED |
Indicates the time that the hazard was fixed. |
|
TIME_SECURED |
Indicates the time that the hazard was made secure. |
|
TIME_PUBLIC_SAFETY_ARR |
The time a public safety official arrived at the hazard scene. |
|
TIME_PUBLIC_SAFETY_REL |
The time a public safety official was relieved from the hazard scene. |
|
REMARKS |
Notes from the operator or dispatcher. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
CANCEL_REASON |
Reason the hazard was cancelled. |
|
CHANGE_DATE |
The time and date an operation was performed on the callback record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident device. |
|
ADDRESS |
The address where the incident is located |