RX_INCIDENT_FEATURES_HISTORY
|
Field Name |
Description |
|---|---|
|
INCIDENT_FEATURE_ID |
The unique identifier assigned to the incident feature. This field corresponds to the ID field in the RX_INCIDENT_FEATURES table. |
|
OID |
Object ID of the feature associated with the incident. |
|
FCID |
Feature class ID of the feature associated with the incident. |
|
SUBID |
The unique ID of each segment of a complex edge. |
|
X |
The x-coordinate of the incident feature. |
|
Y |
The y-coordinate of the incident feature. |
|
INCIDENT_ID |
The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table. |
|
TIME_REPORTED |
Time that the feature was reported out. |
|
CONFIRMED |
Indicates whether the feature has been confirmed out. This field uses the CONFIRMED domain. |
|
FACILITY_ID |
The Facility ID of the incident feature as defined in the geodatabase. |
|
USER_CREATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record. |
|
USER_UPDATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
REMARKS |
Notes from the operator or dispatcher. |
|
CHANGE_DATE |
The date an operation was performed on the incident record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |
|
CANCEL_REASON |
Reason the feature was cancelled. |
|
ADDRESS |
The address where the incident is located |