IFE Interface Generic Commands
Get Current Time
The get current time command is not hardware protected. The get current time command is still enabled when the locking pad located on the front panel on the IFE interface is in locked position.
To get the current time for all modules, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
768 |
Command code = 768 |
|
0x1F40 |
8001 |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
INT16U |
8704 |
Destination = 8704 (0x2200) |
|
0x1F42 |
8003 |
– |
INT16U |
0 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
0 |
Password of the command = 0 (no password required) |
The following registers contain the time data:
-
Register 8023 holds the month in the MSB, the day in the LSB.
-
Register 8024 holds the year offset in the MSB (add 2000 to get the year) and the hour in the LSB.
-
Register 8025 holds the minutes in the MSB, the seconds in the LSB.
-
Register 8026 holds the milliseconds.
Set Absolute Time
The set absolute time command is still enabled when the locking pad located on the front panel on the IFE interface is in locked position.
To set the absolute time for all the IMU modules, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
769 |
Command code = 769 |
|
0x1F40 |
8001 |
– |
INT16U |
18 |
Number of parameters (bytes) = 18 |
|
0x1F41 |
8002 |
– |
INT16U |
8704 |
Destination = 8704 (0x2200) |
|
0x1F42 |
8003 |
– |
INT16U |
0 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
0 |
Password of the command = 0 (no password required) |
|
0x1F45-0x1F48 |
8006–8009 |
– |
XDATE |
– |
Current date/time |
Read IMU Name and Location
To read the IMU name and location, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
1024 |
Command code = 1024 |
|
0x1F40 |
8001 |
– |
INT16U |
16 |
Number of parameters (bytes) = 16 |
|
0x1F41 |
8002 |
– |
INT16U |
8704 |
Destination = 8704 (0x2200) |
|
0x1F42 |
8003 |
– |
INT16U |
0 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
0 |
Password of the command = 0 (no password required) |
|
0x1F45–0x1F46 |
8006–8007 |
– |
INT32U |
– |
|
|
0x1F47 |
8008 |
– |
INT16U |
2048 |
2048 |
The IMU name and location is returned to command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F53 |
8020 |
– |
INT16U |
1024 |
Last command code |
|
0x1F54 |
8021 |
– |
INT16U |
– |
Command status:
|
|
0x1F55 |
8022 |
– |
INT16U |
– |
Number of bytes returned (0 if command failed) |
|
0x1F56 |
8023 |
– |
OCTET STRING |
8704 |
If command succeeded:
|
|
0x1F57–0x1F6D |
8024–8046 |
– |
OCTET STRING |
– |
Depends on the length of the IMU name or location and ends by the NULL character 0x00 |
Write IMU Name and Location
The IMU name and location can be read from registers 11801 to 11868.
To write the IMU name and location, set the command registers the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
1032 |
Command code = 1032 |
|
0x1F40 |
8001 |
– |
INT16U |
16–62 |
Number of parameters (bytes) = depends on the length of the IMU name or location (up to 46 characters) |
|
0x1F41 |
8002 |
– |
INT16U |
0 |
Destination = 0 (0x0000) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45–0x1F46 |
8006–8007 |
– |
INT32U |
– |
|
|
0x1F46 |
8008 |
– |
INT16U |
2048 |
2048 |
|
0x1F48 |
8009 |
– |
OCTET STRING |
– |
|
|
0x1F49–0x1F5F |
8010–8038 |
– |
OCTET STRING |
– |
Depends on the length of the IMU name or location and ends by the NULL character 0x00 |
Set Validity Duration of Data
This command allows to set the validity duration of data in the standard and legacy datasets.
The validity duration of data can be read in a register Validity Duration of Data.
To set the validity duration of data, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41868 |
Command code = 41868 |
|
0x1F40 |
8001 |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
INT16U |
8705 |
Destination = 8705 (0x2201) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator, Services, Engineer, or Operator user profile password |
|
0x1F45 |
8006 |
s |
INT16U |
5–300 (in step of 5 s) |
Validity duration of data Factory setting: 10 s |