IFE Interface Identification and Status Registers
IFE Interface Firmware Revision
The IFE interface firmware revision starts at register 11776 and has a maximum length of eight registers.
The firmware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2DDF–0x2DEE |
11744–11759 |
R |
– |
OCTET STRING |
– |
Device family |
|
0x2DEF–0x2DF6 |
11760–11767 |
R |
– |
OCTET STRING |
– |
Product range |
|
0x2DF7–0x2DFE |
11768–11775 |
R |
– |
OCTET STRING |
– |
Product model |
|
0x2DFF–0x2E04 |
11776–11781 |
R |
– |
OCTET STRING |
– |
Firmware revision |
IFE Interface Hardware Revision
The IFE interface hardware revision starts at register 11784 and has a maximum length of eight registers.
The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E07–0x2E0C |
11784–11789 |
R |
– |
OCTET STRING |
– |
Hardware revision |
IMU Identification
Identification of the IMU can be set by using the EcoStruxure Power Commission software. When not programmed, the IMU identification registers return 0 (0x0000).
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E2F–0x2E38 |
11824–11833 |
R-WC |
– |
OCTET STRING |
– |
User application name set by using:
Device name used for acquiring the IP address using DHCP and also the friendly name on DPWS device discovery. Example: ‘IFE-0A129F’ Maximum length is 64 characters |
|
0x2E18–0x2E2E |
11801–11823 |
R |
OCTET STRING |
– |
IMU name (for ComPacT NS/NSX and PowerPacT only) |
|
|
0x2E2F–0x2E38 |
11824–11833 |
R |
– |
OCTET STRING |
– |
Vendor name = ‘Schneider Electric’ |
|
0x2E39–0x2E42 |
11834–11843 |
R |
– |
OCTET STRING |
– |
Product code:
|
|
0x2E43–0x2E44 |
11844–11845 |
– |
– |
– |
– |
Reserved |
|
0x2E45–0x2E5B |
11846–11868 |
R-RC-WC |
– |
OCTET STRING |
– |
IMU location (for ComPacT NS/NSX and PowerPacT only) = up to 45 ASCII characters ended by the NULL character 0x00 |
Locking Pad Position
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E72 |
11891 |
R |
– |
INT16U |
1,3 |
Locking pad position
|
Current Date and Time
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E73–0x2E76 |
11892–11895 |
R-WC |
– |
DATETIME |
– |
Current date and time in DATETIME format |
|
0x2E77–0x2E78 |
11896–11897 |
R |
Seconds |
INT32U |
0x00–0xFFFFFFFF |
Number of seconds counted since last start |
Product Identification
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E7C |
11901 |
R |
– |
INT16U |
17100–17101 |
Product identification:
|
Validity Duration of Data
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x306A |
12395 |
R |
s |
INT16U |
5–300 (in step of 5 s) |
Duration of validity of data in the dataset |
Read Device Identification
The Read Device Identification function is used to access in a standardized manner the information required to identify a device clearly. The description is made up of a set of objects (ASCII character strings).
A complete description of the Read Device Identification function is available at www.modbus.org.
The coding for the identification of the IFE interface is the following:
|
Name |
Type |
Description |
|---|---|---|
|
Vendor name |
OCTET STRING |
‘Schneider Electric’ (18 characters) |
|
Product code |
OCTET STRING |
|
|
Firmware revision |
OCTET STRING |
‘XXX.YYY.ZZZ’ |
|
Vendor URL |
OCTET STRING |
‘www.se.com’ (26 characters) |
|
Product name |
OCTET STRING |
|
|
Family |
OCTET STRING |
‘Gateway and server’ |
|
Range |
OCTET STRING |
‘Enerlin’X’ |
|
Model |
OCTET STRING |
‘IFE Ethernet interface’ or ‘IFE/Gateway’ |
|
Product ID |
INT16U |
Product ID of the core of IMU:
|
MAC Address of the IFE Server
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E7D–0x2E7F |
11902–11904 |
R |
– |
INT16U |
– |
MAC address of the IFE interface coded over 3 registers (6 bytes) in hexadecimal. Example: The MAC address 00:80:F4:02:12:34 (or 00-80-F4-02-12-34) is coded in hexadecimal as follows: 0080F4021234 (0x00 0x80 0xF4 0x02 0x12 0x34). |
Manufacturing Date and Time
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E89–0x2E8C |
11914–11917 |
R |
– |
DATETIME |
– |
Manufacturing date and time |
IFE Interface Serial Number
The IFE interface serial number is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.
-
PP = plant code
-
YY = year of fabrication (05–99)
-
WW = week of fabrication (01–53)
-
D = day of fabrication (1–7)
-
nnnn = production number of the device on the day (0001–9999)
A read request of 6 registers is necessary to read the IFE interface serial number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x02E91 |
11922 |
R |
– |
OCTET STRING |
– |
‘PP’ |
|
0x02E92 |
11923 |
R |
– |
OCTET STRING |
‘05’–‘99’ |
‘YY’ |
|
0x02E93 |
11924 |
R |
– |
OCTET STRING |
‘01’–‘53’ |
‘WW’ |
|
0x02E94 |
11925 |
R |
– |
OCTET STRING |
D: ‘1’–‘7’ n: ‘0’–‘9’ |
‘Dn’ |
|
0x02E95 |
11926 |
R |
– |
OCTET STRING |
‘00’–‘99’ |
‘nn’ |
|
0x02E96 |
11927 |
R |
– |
OCTET STRING |
‘0’–‘9’ |
‘n’ (the NULL character ends the serial number) |
Modbus Parameters of the IFE Server
These parameters are valid for the IFE switchboard server only.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x306F |
12400 |
R |
– |
INT16U |
– |
Modbus address of IFE server (always 255) |
|
0x3070 |
12401 |
R |
– |
INT16U |
1–3 |
Modbus parity:
|
|
0x3071 |
12402 |
R |
– |
INT16U |
5–8 |
Modbus Baud rate:
|
|
0x3072 |
12403 |
R |
– |
INT16U |
1,3,5 |
Number of stop bits:
|
Time Synchronization
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3098–0x30B7 |
12441–12472 |
R |
– |
OCTET STRING |
– |
The type of source use for time synchronization:
|
|
0x30B8–0x30BB |
12473–12476 |
R |
– |
DATETIME |
– |
Date and time of last time synchronization |
|
0x30BC–0x30BD |
12477–12478 |
R |
s |
FLOAT32 |
– |
Time since last time synchronization |
|
0x30BE |
12479 |
R |
– |
INT16U |
0–2 |
Status of automatic time synchronization:
|
|
0x30BF |
12480 |
R |
– |
INT16 |
– |
SNTP fails count |