IP Network Parameters
Network Parameters
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x27FF–0x2800 |
10240–10241 |
R |
– |
INT32 |
0–1 |
Network configuration mode:
|
IPv4 Parameters
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2823–0x2824 |
10276–10277 |
R-WC |
– |
INT32U |
0–2 |
IPv4 address acquisition mode, set by using the EcoStruxure Power Commission software:
|
|
0x2825–0x2826 |
10278–10279 |
R |
– |
INT32U |
– |
IPv4 address acquisition status:
|
|
0x2827–0x2828 |
10280–10281 |
R-WC |
– |
INT32U |
– |
IPv4 address of IFE interface Example: 169.254.1.1 Register 10280 = 0xA9FE Register 10281 = 0x0101 |
|
0x2829–0x282A |
10282–10283 |
R-WC |
– |
INT32U |
– |
IPv4 subnet mask Example: 255.255.0.0 Register 10282 = 0xFFFF Register 10283 = 0x0000 |
|
0x282B–0x282C |
10284–10285 |
R-WC |
– |
INT32U |
– |
IPv4 default gateway address Example: 169.154.1.1 Register 10284 = 0xA9FE Register 10285 = 0x0101 |
|
0x282D–0x2846 |
10286–10311 |
– |
– |
– |
– |
Reserved |