Modbus Network Parameters
Modbus Locking Pad Position
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E72 |
11891 |
R |
– |
INT16U |
1–3 |
Modbus locking pad position
|
Validity Duration of Data
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x306A |
12395 |
R |
s |
INT16U |
5–300 (in step of 5 s) |
Duration of validity of data in the dataset |
Auto-Speed Sensing State
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x306E |
12399 |
R |
– |
INT16U |
0–1 |
Auto-Speed sensing state
|
IFM Interface Modbus Address
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x306F |
12400 |
R |
– |
INT16U |
1–99 |
IFM interface Modbus address |
Modbus Parity
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3070 |
12401 |
R |
– |
INT16U |
1–3 |
Modbus parity
|
Modbus Baud Rate
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3071 |
12402 |
R |
– |
INT16U |
5–8 |
Modbus Baud rate
|
Number of Stop Bits
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3072 |
12403 |
R |
– |
INT16U |
0–5 |
Number of stop bits
|