Basic Protection Parameters
Neutral Protection Parameters
The neutral protection is only available when system type in register 3314 is 30 or 41.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2230 |
8753 |
RW |
1 |
– |
INT16U |
0–3 |
A/E/P |
Type of neutral protection: (1) 0 = OFF 1 = N/2 (Ir/2) 2 = N (Ir) 3 = Nx1.6 (1.6 Ir) (2) |
|
(1) Write Access only with MicroLogic P trip unit. (2) Value accessible only for MicroLogic P trip unit. |
||||||||
Long-Time Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2231 |
8754 |
R |
– |
– |
INT16U |
0–1 |
A/E/P |
– |
Status: 0x0001 = On |
|
0x2232 |
8755 |
RW |
– |
– |
INT16U |
– |
– |
– |
Type of IDMTL curve (1) |
|
A/E/P |
0 |
Standard long-time curve I2t (factory setting) |
|||||||
|
P |
1 |
SIT curve |
|||||||
|
P |
2 |
VIT curve |
|||||||
|
P |
3 |
EIT (I2t on) curve |
|||||||
|
P |
4 |
HVF curve |
|||||||
|
P |
5 |
Constant time (I2t off) |
|||||||
|
– |
6–15 |
Reserved |
|||||||
|
0x2233–0x2234 |
8756–8757 |
RW |
1 |
A |
MOD 10000 |
40–8000 |
A/E/P |
– |
Ir pick-up value (1) |
|
0x2235 |
8758 |
RW |
1 |
ms |
INT16U |
500–24000 |
A/E/P |
– |
tr time delay (1) |
|
0x2236–0x223A |
8759-8763 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) Write Access only with MicroLogic P trip unit. |
|||||||||
Short-Time Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x223B |
8764 |
R |
– |
– |
INT16U |
0–1 |
A/E/P |
– |
Status: 0x0001 = On |
|
0x223C |
8765 |
RW |
– |
– |
INT16U |
0–1 |
A/E/P |
– |
Type of protection: (1) 0 = I2t On 1 = I2t Off |
|
0x223D–0x223E |
8766–8767 |
RW |
1 |
A |
MOD 10000 |
60–80 000 |
A/E/P |
– |
Isd pick-up value (1) |
|
0x223F |
8768 |
RW |
1 |
ms |
INT16U |
0–400 |
A/E/P |
– |
tsd time delay (1) 0 s: valid only for the I²t off position 100–400 ms: valid for the I²t on and I²t off positions |
|
0x2240–0x2244 |
8769–8773 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) Write Access only with MicroLogic P trip unit. |
|||||||||
Instantaneous Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2245 |
8774 |
R |
– |
– |
INT16U |
0x0001–0x0101 |
A/E/P |
– |
0x0001 = protection active (factory setting) 0x0101 = protection OFF |
|
0x2246 |
8775 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x2247–0x2248 |
8776–8777 |
RW |
1 |
A |
MOD 10000 |
200–120000 |
A/E/P |
– |
I pick-up value for the instantaneous protection (1) |
|
0x2249– 0x224E |
8778–8783 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) Write Access only with MicroLogic P trip unit. |
|||||||||
Ground-Fault Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x224F |
8784 |
RW |
– |
– |
INT16U |
0x0001–0x0101 |
A/E/P |
– |
Protection status: (1) (2) 0x0001 = protection active (factory setting) 0x0101 = protection OFF |
|
0x2250 |
8785 |
RW |
– |
– |
INT16U |
0–1 |
A/E/P |
– |
Type of protection: (1) 0 = I2t On 1 = I2t Off |
|
0x2251–0x2252 |
8786–8787 |
RW |
1 |
A |
MOD 10000 |
30–1200 |
A/E/P |
– |
Ig pickup for the ground-fault protection (1) |
|
0x2253 |
8788 |
RW |
1 |
ms |
INT16U |
0–400 |
A/E/P |
– |
tg tripping time delay for the ground-fault protection: (1) 0 s = valid only for the I2t off position 100–400 ms = valid for the I2t on and I2t off positions |
|
0x2254–0x2258 |
8789–8793 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) Write Access only with MicroLogic P trip unit. (2) In order to be able to write this register, the following conditions must be met:
|
|||||||||
Earth-Leakage (Vigi) Protection Parameters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2259 |
8794 |
R |
– |
– |
INT16U |
0x0001 |
A/P |
– |
0x0001 = protection active |
|
0x225A |
8795 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x225B–0x225C |
8796–8797 |
RW |
1 |
mA |
MOD 10000 |
5–300 |
A/P |
– |
IΔn pickup for the earth-leakage protection (1) |
|
0x225D |
8798 |
RW |
1 |
ms |
INT16U |
0–1000 |
A/P |
– |
Δt tripping time delay for the earth-leakage protection (1) |
|
0x225E–0x2262 |
8799–8803 |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) Write Access only with MicroLogic P trip unit. |
|||||||||