Applications
IO Application Status
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3927 |
14632 |
R |
– |
INT16U |
– |
0 |
Cradle application enabled or disabled:
|
|
1–15 |
Reserved |
||||||
|
0x3928 |
14633 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14632:
|
Cradle Management
The table describes the registers related to the cradle management application performed by IO 1 (predefined or user defined application).
The registers 18300–18329 are related to the cradle management application performed by IO 2 (predefined or user defined application).
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3BC3 |
15300 |
R-RC |
– |
INT16U |
– |
– |
Quality of each bit of register 15301:
|
|
0x3BC4 |
15301 |
R-RC |
– |
INT16U |
– |
– |
Cradle status |
|
0–7 |
Reserved |
||||||
|
8 |
Device in disconnected position (CD) |
||||||
|
9 |
Device in connected position (CE) |
||||||
|
10 |
Device in the test position (CT) |
||||||
|
11–15 |
Reserved |
||||||
|
0x3BC5–0x3BC6 |
15302–15303 |
R-RC-WC |
– |
INT32U |
0–65534 |
– |
Cradle connected position counter This counter increments for each rising edge of the cradle connected position |
|
0x3BC7–0x3BC8 |
15304–15305 |
R-RC-WC |
– |
INT32U |
0–65534 |
– |
Cradle disconnected position counter This counter increments for each rising edge of the cradle disconnected position |
|
0x3BC9–0x3BCA |
15306–15307 |
R-RC-WC |
– |
INT32U |
0–65534 |
– |
Cradle test position counter This counter increments for each rising edge of the cradle test position |
|
0x3BCB–0x3BCE |
15308–15311 |
R-RC |
– |
DATETIME |
– |
– |
Timestamp of the last change for the cradle connected position |
|
0x3BCF–0x3BD2 |
15312–15315 |
R-RC |
– |
DATETIME |
– |
– |
Timestamp of the last change for the cradle disconnected position |
|
0x3BD3–0x3BD6 |
15316–15319 |
R-RC |
– |
DATETIME |
– |
– |
Timestamp of the last change for the cradle test position |
|
0x3BD7–0x3BD8 |
15320–15321 |
R-WC |
s |
INT32U |
– |
– |
Operating time since last grease maintenance |
|
0x3BD9–0x3BDA |
15322–15323 |
R-WC |
s |
INT32U |
– |
– |
Operating time since last move connected position |
|
0x3BDB |
15324 |
R |
– |
INT16U |
0-65534 |
– |
Cradle contact regrease counter |
|
0x3BDC–0x3BE0 |
15325–15329 |
– |
– |
– |
– |
– |
Reserved |
Drawer Management
The table describes the registers related to the Drawer management user-defined application performed by IO 1.
The registers 18330–18359 are related to the Drawer management user-defined application performed by IO 2.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3BE1 |
15330 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 15331: 0 = Invalid 1 = Valid |
|
0x3BE2 |
15331 |
R |
– |
INT16U |
– |
– |
Drawer status |
|
0–7 |
Reserved |
||||||
|
8 |
Drawer in disconnected position |
||||||
|
9 |
Drawer in connected position |
||||||
|
10 |
Drawer in the test position |
||||||
|
11–15 |
Reserved |
||||||
|
0x3BE3–0x3BE4 |
15332–15333 |
R |
– |
INT32U |
– |
– |
Drawer connected position counter. This counter increments for each rising edge of the drawer connected position. |
|
0x3BE5–0x3BE6 |
15334–15335 |
R |
– |
INT32U |
– |
– |
Drawer disconnected position counter. This counter increments for each rising edge of the drawer disconnected position. |
|
0x3BE7–0x3BE8 |
15336–15337 |
R |
– |
INT32U |
– |
– |
Drawer test position counter. This counter increments for each rising edge of the drawer test position. |
|
0x3BE9–0x3BEC |
15338–15341 |
R |
– |
DATETIME |
– |
– |
Timestamp of the last change for the drawer connected position. |
|
0x3BED–0x3BF0 |
15342–15345 |
R |
– |
DATETIME |
– |
– |
Timestamp of the last change for the drawer disconnected position. |
|
0x3BF1–0x3BF4 |
15346–15349 |
R |
– |
DATETIME |
– |
– |
Timestamp of the last change for the drawer test position. |
|
0x3BF5–0x3BFE |
15350–15359 |
– |
– |
– |
– |
– |
Reserved |
Light Control
The table describes the registers related to the Light control predefined application performed by IO 1.
The registers 18400–18409 are related to the Light control predefined application performed by IO 2.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3C27 |
15400 |
R |
– |
INT16U |
0–1 |
Quality of register 15401:
|
|
0x3C28 |
15401 |
R |
– |
INT16U |
0–1 |
Light status:
|
|
0x3C29–0x3C2A |
15402–15403 |
R |
s |
INT32U |
0–54000 |
Remaining time in ON or OFF state (depending of the light status) |
|
0x3C2B– |
15404 |
R |
– |
INT16U |
0–2 |
Light simple command(1):
|
|
0x3C2C–0x3C30 |
15405–15409 |
– |
– |
– |
– |
Reserved |
|
(1) Simple commands are enabled by factory setting. The simple commands can be disabled by using the command Enable/Disable simple commands. |
||||||
Load Control
The table describes the registers related to the Load control predefined application performed by IO 1.
The registers 18410–18419 are related to the Load control predefined application performed by IO 2.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x3C31 |
15410 |
R |
– |
INT16U |
0–1 |
Quality of register 15411:
|
|
0x3C32 |
15411 |
R |
– |
INT16U |
0–1 |
Load status:
|
|
0x3C33–0x3C34 |
15412–15413 |
R |
s |
INT32U |
0–54000 |
Remaining time in ON or OFF state (depending of the load status) |
|
0x3C35 |
15414 |
R |
– |
INT16U |
0–2 |
Load simple command(1):
|
|
0x3C36–0x3EEC |
15415–16109 |
– |
– |
– |
– |
Reserved |
|
(1) Simple commands are enabled by factory setting. The simple commands can be disabled by using the command Enable/Disable simple commands. |
||||||