Digital Input and Output Status
Addresses and Registers List
The following table describes the digital inputs and outputs status addresses, and registers regarding the IO module.
|
IO Module |
Addresses |
Registers |
|---|---|---|
|
IO 1 |
0x3905–0x3908 |
14598–14601 |
|
IO 2 |
0x44BD–0x44C0 |
17598–17601 |
Digital Input and Output Status Registers for IO 1
The order and the description of the digital input and output status registers for IO 2 are the same as those of IO 1.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3905 |
14598 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14599:
|
|
0x3906 |
14599 |
R |
– |
INT16U |
– |
– |
Digital input status register:
|
|
0 |
I1 status |
||||||
|
1 |
I2 status |
||||||
|
2 |
I3 status |
||||||
|
3 |
I4 status |
||||||
|
4 |
I5 status |
||||||
|
5 |
I6 status |
||||||
|
6–15 |
Reserved |
||||||
|
0x3907 |
14600 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 14601:
|
|
0x3908 |
14601 |
R–WC |
– |
INT16U |
– |
– |
Digital output status register:
|
|
0 |
O1 status |
||||||
|
1 |
O2 status |
||||||
|
2 |
O3 status |
||||||
|
3–15 |
Reserved |