Miscellaneous
Nominal Current
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x222D |
8750 |
R |
1 |
A |
INT16U |
0–8000 |
A/E/P |
Rated circuit breaker current Factory setting = 100 A (circuit breaker sensor plug not present) |
Protection Manager Measurements
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2263 |
8804 |
R |
– |
– |
INT16U |
0–65535 |
P |
Protection Manager (PM) configuration change counter This counter is incremented each time a PM setting change is applied through HMI (keyboard or switches) or COM. If switches were changed during power off, this counter is incremented at power-up. |
|
0x2280 |
8833 |
R |
10 |
%In |
INT16U |
0–16000 |
P |
Maximum fault current (trip) recorded on phase 1 since last reset (4) Factory setting = 0x8000 (no fault recorded or circuit breaker type not entered) |
|
0x2281 |
8834 |
R |
10 |
%In |
INT16U |
0–16000 |
P |
Maximum fault current (trip) recorded on phase 2 since last reset (4) Factory setting = 0x8000 (no fault recorded or circuit breaker type not entered) |
|
0x2282 |
8835 |
R |
10 |
%In |
INT16U |
0–16000 |
P |
Maximum fault current (trip) recorded on phase 3 since last reset (4) Factory setting = 0x8000 (no fault recorded or circuit breaker type not entered) |
|
0x2283 |
8836 |
R |
10 |
%In |
INT16U |
0–16000 |
P |
Maximum fault current (trip) recorded on the neutral since last reset (4) Factory setting = 0x8000 (no fault recorded or circuit breaker code not supplied) |
|
0x2284 |
8837 |
R |
1 |
%Ir |
INT16U |
0–32767 |
A/P |
RMS current on phase 1 expressed as a % of the Ir long-time pick-up value |
|
0x2285 |
8838 |
R |
1 |
%Ir |
INT16U |
0–32767 |
A/P |
RMS current on phase 2 expressed as a % of the Ir long-time pick-up value |
|
0x2286 |
8839 |
R |
1 |
%Ir |
INT16U |
0–32767 |
A/P |
RMS current on phase 3 expressed as a % of the Ir long-time pick-up value |
|
0x2287 |
8840 |
R |
1 |
%Ir |
INT16U |
0–32767 |
A/P |
RMS current on the neutral expressed as a % of the rated current In x the selected neutral setting (x 1, x 2 or x 0.5) (1) |
|
0x2288 |
8841 |
R |
1 |
%Ig |
INT16U |
0–32767 |
A/P |
"Residual" ground-fault current expressed as a % of the Ig ground-fault protection pick-up value (2) |
|
0x2289 |
8842 |
R |
100 |
%Idn |
INT16U |
0–32767 |
A/P |
Earth-leakage current expressed as a % of the IΔN earth-leakage protection pick-up value (3) |
|
(1) Value not accessible when configuration register 9618 selects "no external CT". (2) Accessible only with MicroLogic 6.0 trip unit. (3) Accessible only with MicroLogic 7.0 trip unit. (4) Auxiliary power is required to calculate the fault currents. Calculation is effective only when the circuit breaker selection code has been supplied (see the MicroLogic P trip units user guide). |
||||||||
Battery Status
The following table represents the battery charge status:
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x228A |
8843 |
R |
1 |
% |
INT16U |
0–100 |
A/E/P |
Battery-charge indicator: 100 % = U > 2800 mV 50 % = 2200 < U < 2800 mV 0 % = U < 2200 mV |
Time Remaining Until Long-Time Tripping
Time remaining until long-time tripping is evaluated every second. If another protection is tripped, then time remaining until long-time tripping continues to be evaluated.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x22A0–0x22A1 |
8865–8866 |
R |
10 |
s |
MOD 10000 |
– |
P |
Time remaining until long-time tripping |
Phase Rotation
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x22A7 |
8872 |
R |
– |
– |
INT16U |
– |
P |
Phase rotation: 0 = ABC (123) 1 = ACB (132) |
Language
This register sets the language used by the trip unit. It may be modified through the trip unit keypad. The factory setting is English but it may be factory set if necessary.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x258D |
9614 |
RW |
– |
– |
INT16U |
– |
P |
0 |
French |
|
1 |
US English |
||||||||
|
2 |
UK English |
||||||||
|
3 |
German |
||||||||
|
4 |
Spanish |
||||||||
|
5 |
Italian |
||||||||
|
7 |
Chinese |
||||||||
|
8 |
Russian |
||||||||
|
9 |
Optional language available on order from Schneider Electric |
||||||||
|
10–15 |
Reserved |
Nominal Frequency
This register rates the circuit breaker operating frequency required by the protection manager to disable phase rotation protection for 400 Hz distribution system.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x258E |
9615 |
RW |
– |
– |
INT16U |
– |
P |
0 |
50 / 60 Hz (factory setting) |
|
1–2 |
Reserved |
||||||||
|
3 |
400 Hz |
||||||||
|
4–15 |
Reserved |