Demand Measurements
General Description
Demand registers include:
-
current demand
-
active, reactive, and apparent power demand
The window duration of current demand depends on the configuration of register 3352. Refer to Demand Time.
The window duration and the window type of power demand depend on the configuration of registers 3354 and 3355. Refer to Demand Time.
-
For the block window, the demand value is updated at the end of the window.
-
For the sliding window,
-
If window duration is configured for less or equal to 15 minutes, the demand value is updated every 15 seconds.
-
If window duration is configured for more than 15 minutes, the demand value is updated every 1 minute.
-
The reset minimum/maximum command (command code = 46728) can reset the content of the peak demand measurement registers.
Current Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0897 |
2200 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Current demand on phase 1: I1 Dmd (2) |
|
0x0898 |
2201 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Current demand on phase 2: I2 Dmd (2) |
|
0x0899 |
2202 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Current demand on phase 3: I3 Dmd (2) |
|
0x089A |
2203 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Current demand on the neutral: IN Dmd (1) (2) |
|
0x089B |
2204 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Maximum current demand on phase 1 since the last reset: I1 Peak Dmd |
|
0x089C |
2205 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Maximum current demand on phase 2 since the last reset: I2 Peak Dmd |
|
0x089D |
2206 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Maximum current demand on phase 3 since the last reset: I3 Peak Dmd |
|
0x089E |
2207 |
R |
1 |
A |
INT16U |
0–32767 |
E/P |
Maximum current demand on the neutral since the last reset: IN Peak Dmd (1) |
|
(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. (2) Only the thermal algorithm is available with MicroLogic E trip units while MicroLogic P trip units have both the thermal and arithmetical mean algorithms. |
||||||||
Active Power Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x08AF |
2224 |
R |
1 |
kW |
INT16U |
0–32767 |
E/P |
Total active power demand: P Dmd (1) (3) |
|
0x08B0 |
2225 |
R |
1 |
kW |
INT16U |
0–32767 |
E/P |
Maximum total active power demand since the last reset: P Peak Dmd |
|
0x08B1 |
2226 |
R |
1 |
kW |
INT16U |
0–32767 |
P |
Predicted active power demand at the end of the window (2) |
|
0x08B2 |
2227 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
P |
Total power factor at last active power demand maximum |
|
0x08B3 |
2228 |
R |
1 |
kVAR |
INT16U |
0–32767 |
P |
Reactive power demand at last active power demand maximum |
|
0x08B4 |
2229 |
R |
1 |
kVA |
INT16U |
0–32767 |
P |
Apparent power demand at last active power demand maximum |
|
(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every 15 seconds. (2) Value is updated every 15 seconds for both block window and sliding window types. (3) Only the thermal algorithm is available with MicroLogic E trip units while MicroLogic P trip units has both the thermal and arithmetical mean algorithms. |
||||||||
Reactive Power Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x08B5 |
2230 |
R |
1 |
kVAR |
INT16U |
0–32767 |
P |
Total reactive power demand: Q Dmd (1) |
|
0x08B6 |
2231 |
R |
1 |
kVAR |
INT16U |
0–32767 |
P |
Reactive power demand maximum since the last reset: Q Peak Dmd |
|
0x08B7 |
2232 |
R |
1 |
kVAR |
INT16U |
0–32767 |
P |
Predicted reactive power demand at the end of the window (2) |
|
0x08B8 |
2233 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
P |
Total power factor at last reactive power demand maximum |
|
0x08B9 |
2234 |
R |
1 |
kW |
INT16U |
0–32767 |
P |
Active power demand at last reactive power demand maximum |
|
0x08BA |
2235 |
R |
1 |
kVA |
INT16U |
0–32767 |
P |
Apparent power demand at last reactive power demand maximum |
|
(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every 15 seconds. (2) Value is updated every 15 seconds for both block window and sliding window types. |
||||||||
Apparent Power Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x08BB |
2236 |
R |
1 |
kVA |
INT16U |
0–32767 |
E/P |
Total apparent power demand: S Dmd (1) |
|
0x08BC |
2237 |
R |
1 |
kVA |
INT16U |
0–32767 |
E/P |
Maximum total apparent power demand since last reset: S Peak Dmd |
|
0x08BD |
2238 |
R |
1 |
kVA |
INT16U |
0–32767 |
P |
Predicted apparent power demand at the end of the window (2) |
|
0x08BE |
2239 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
P |
Total power factor at last apparent power demand maximum |
|
0x08BF |
2240 |
R |
1 |
kW |
INT16U |
0–32767 |
P |
Active power demand at last apparent power demand maximum |
|
0x08C0 |
2241 |
R |
1 |
kVAR |
INT16U |
0–32767 |
P |
Reactive power demand at last apparent power demand maximum |
|
(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every 15 seconds. (2) Value is updated every 15 seconds for both block window and sliding window types. |
||||||||