MicroLogic Trip Unit Identification
Identification of the Metering Manager
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0CE6–0x0CE7 |
3303–3304 |
RW |
– |
– |
OCTET STRING |
0x00–0x7F |
P |
Short identifier of the metering manager, coded over 4 ASCII characters. Factory setting: |
|
0x0CE8–0x0CEF |
3305–3312 |
RW |
– |
– |
OCTET STRING |
0x00–0x7F |
P |
Long identifier of the metering manager, coded over 16 ASCII characters. Factory setting: |
Serial Number
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x21FB–0x21FE |
8700–8703 |
R |
1 |
– |
OCTET STRING |
– |
A/E/P |
Serial number encoded in ASCII |
Hardware Version
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2204 |
8709 |
R |
– |
– |
INT16U |
0x0000–0xFFFF |
P |
Hardware version of the MicroLogic trip unit. |
Firmware Version
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2205 |
8710 |
R |
1 |
– |
INT16 |
– |
A/E/P |
MicroLogic trip unit firmware version. For example, the value 8244 corresponds to version 8.244. |
Product Identification
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x220B |
8716 |
R |
1 |
– |
INT16U |
15133–15137 |
A/E/P |
Product identification with the protection manager: 15131 = MicroLogic A 15137 = MicroLogic E 15133 = MicroLogic P |
|
0x0EE7 |
3816 |
R |
1 |
– |
INT16U |
15134–15138 |
E/P |
Product identification with the metering manager: 15138 = MicroLogic E 15134 = MicroLogic P |
Protection Type
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2223 |
8740 |
R |
1 |
– |
OCTET STRING |
20–70 |
A/E/P |
Type of protection: ‘20’= MicroLogic 2.0 ‘30’= MicroLogic 3.0 ‘40’= MicroLogic 4.0 ‘50’= MicroLogic 5.0 ‘60’= MicroLogic 6.0 ‘70’= MicroLogic 7.0 |
Metering Type
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2224 |
8741 |
R |
1 |
– |
OCTET STRING |
0x2041–0x204D |
A/E/P |
Type of measurement: 0x2041 = ‘space’ and ‘A’ 0x2045 = ‘space’ and ‘E’ 0x2050 = ‘space’ and ‘P’ Or type of application: 0x204D = ‘space’ and ‘M’ |
Long-Time Rating Plug
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2225 |
8742 |
R |
1 |
– |
INT16U |
0–15 |
A/E/P |
Type of long-time rating plug: 0 = missing 1 = IEC standard 2 = IEC low 3 = IEC High 7 = UL-A 8 = UL-B 9 = UL-C 10 = OFF 11 = UL-D 12 = UL-E 13 = UL-F 14 = UL-G 15 = UL-H |
Identification of the Protection Manager
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2583–0x2584 |
9604–9605 |
RW |
– |
– |
OCTET STRING |
– |
P |
Short identifier of the protection manager, coded over 4 ASCII characters. Factory setting: |
|
0x2585–0x258C |
9606–9613 |
RW |
– |
– |
OCTET STRING |
– |
P |
Long identifier of the protection manager, coded over 16 ASCII characters. Factory setting: |
Circuit Breaker Type
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2591 |
9618 |
RW |
– |
– |
INT16U |
0–2 |
P |
0 = 3-pole circuit breaker without external neutral current transformer (factory setting) 1 = 4-pole circuit breaker 2 = 3-pole circuit breaker with external neutral current transformer |
Circuit Breaker Characteristics
The characteristics can be:
-
set by using the MicroLogic HMI in
-
downloaded by using the test kit
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2675 |
9846 |
R |
– |
– |
INT16U |
0–3 |
P |
Standard: 0 = UL 1 = IEC 2 = ANSI 3 = IEC/GB |
|
0x2676 |
9847 |
R |
– |
– |
INT16U |
0–2 |
P |
Type: 0 = MasterPact 1 = ComPact NS 2 = |
|
0x2677–0x267C |
9848–9853 |
R |
– |
– |
OCTET STRING |
– |
P |
ASCII character strings (for example, ‘NT08N’) |