Measurement Configuration Commands
Set Up ENVT Presence
The user can read the ENVT (External Neutral Voltage Tap) presence parameters at register 3314.
To set up ENVT presence, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
46472 |
E/P |
Command code = 46472 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
E/P |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
E/P |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
E/P |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
E/P |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
E/P |
0 = ENVT is not present 1 = ENVT is present |
Reset Minimum/Maximum
The reset minimum/maximum command resets the energy measurements (registers 2000 to 2027).
The reset minimum/maximum command resets the peak demand measurements (registers 2200 to 2241).
To reset minimum/maximum values of measurements, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
46728 |
– |
– |
Command code = 46728 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
– |
– |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
– |
– |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
– |
– |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
– |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
– |
– |
– |
Reset minimum/maximum of metering variables:
|
|
A/E/P |
0 |
Reset minimum/maximum current (I1, I2, I3, IN, Imax, Ig, IΔn, Iavg, and Iunbal) |
||||||
|
E/P |
1 |
Reset minimum/maximum voltage (V12, V13, V23, V1N, V2N, V3N, VavgL-L, VavgL-N, and Vunbal) |
||||||
|
E/P |
2 |
Reset minimum/maximum power (active power, reactive power, apparent power, and distortion power) |
||||||
|
E/P |
3 |
Reset minimum/maximum power factor and cosϕ |
||||||
|
E/P |
4 |
Reset minimum/maximum total harmonic distortion (THD) |
||||||
|
E/P |
5 |
Reset peak of current demand |
||||||
|
E/P |
6 |
Reset peak of active power, reactive power, and apparent power demand |
||||||
|
E/P |
7 |
Reset minimum/maximum frequency |
||||||
|
– |
8 |
Not applicable |
||||||
|
E/P |
9 |
Reset energy (active, reactive, apparent) |
||||||
|
– |
10–15 |
Reserved |
Power Flow Sign Configuration
The user can read the power flow sign configuration at register 3316 Power Flow Sign.
To set the power flow sign parameters, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47240 |
P |
Command code = 47240 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
P |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
P |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
P |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
P |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
P |
Power flow sign: 0 = the active power flows from upstream (top) to downstream (bottom) (factory setting) 1 = the active power flows from downstream (bottom) to upstream (top). |
Power Factor Sign Configuration
The user can read the power factor sign configuration at register 3318.
To set the power factor sign parameters, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47241 |
E |
Command code = 47241 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
E |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
E |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
E |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
E |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–2 |
E |
Sign convention for the power factor and the fundamental power factor (cosϕ): 0 = IEC convention 2 = IEEE convention (factory setting) |
Energy Accumulation Mode Configuration
The user can read the energy accumulation mode configuration at register 3324.
To set the energy accumulation mode parameters, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47242 |
E/P |
Command code = 47242 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
E/P |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
E/P |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
E/P |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
E/P |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
E/P |
Energy accumulation mode: 0 = absolute accumulation (factory setting) 1 = signed accumulation |
Current Demand Configuration
The user can read the duration of the current demand calculation window at register 3352.
The user can read the current demand parameters from register 2200 to 2207.
To start current demand, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47243 |
E/P |
Command code = 47243 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
E/P |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
E/P |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
E/P |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
E/P |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
Min |
INT16U |
5–60 |
E/P |
Duration of the current demand calculation window, adjustable in step of 1. The factory setting is 15 minutes (sliding). |
Power Demand Configuration
The user can read the power demand calculation method from register 3354 to 3355.
The user can read the power demand parameters from register 2224 to 2237.
To start power demand, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47244 |
E/P |
Command code = 47244 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
14 |
E/P |
Number of parameters (bytes) = 14 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
E/P |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
E/P |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
E/P |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–5 |
E/P |
Power demand calculation method (window type): 0 = sliding (factory setting) 2 = fixed 5 = synchronized to communication |
|
0x1F46 |
8007 |
– |
Min |
INT16U |
5–60 |
E/P |
Duration of the power demand calculation window, adjustable in step of 1. The factory setting is 15 minutes. |
Set Up Nominal Primary Voltage Vn Display
The user can read the nominal voltage at register 9616.
To set the nominal primary voltage Vn display parameters, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
47245 |
E/P |
Command code = 47245 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
E/P |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
E/P |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
E/P |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
E/P |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
V |
INT16U |
0–65535 |
E/P |
Nominal primary voltage Vn (factory setting = 690 V) |