Digital Inputs
Digital Input Register Mapping
Each digital input description is made up of 80 registers.The order and the description of the digital inputs 2, 3, 4, 5, and 6 are the same as those of digital input 1.
|
IO Module |
Digital Input Number |
Digital Input Addresses |
Digital Input Registers |
|---|---|---|---|
|
IO 1 |
I1 |
0x3669–0x36B8 |
13930–14009 |
|
I2 |
0x36B9–0x3708 |
14010–14089 |
|
|
I3 |
0x3709–0x3758 |
14090–14169 |
|
|
I4 |
0x3759–0x37A8 |
14170–14249 |
|
|
I5 |
0x37A9–0x37F8 |
14250–14329 |
|
|
I6 |
0x37F9–0x3848 |
14330–14409 |
|
|
IO 2 |
I1 |
0x4221–0x4270 |
16930–17009 |
|
I2 |
0x4271–0x42C0 |
17010–17089 |
|
|
I3 |
0x42C1–0x4310 |
17090–17169 |
|
|
I4 |
0x4311–0x4360 |
17170–17249 |
|
|
I5 |
0x4361–0x43B0 |
17250–17329 |
|
|
I6 |
0x43B1–0x4400 |
17330–17409 |
Digital Input 1 Registers of IO 1
The order and the description of the digital input 1 registers of IO 2 are the same as those of IO 1:
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x3669 |
13930 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 13931:
|
|
0x366A |
13931 |
R |
– |
INT16U |
– |
0 |
Digital input status:
|
|
1 |
Digital input forced status:
|
||||||
|
2–15 |
Reserved |
||||||
|
0x366B–0x366E |
13932–13935 |
R |
– |
DATETIME |
– |
– |
Timestamp for the last input transition:
Valid if input signal type is a normal digital input (not valid for pulse digital input). |
|
0x366F–0x3670 |
13936–13937 |
– |
– |
– |
– |
– |
Reserved |
|
0x3671–0x3672 |
13938–13939 |
R |
– |
INT32U |
0–4294967294 |
– |
Input counter value This counter increments for each rising edge of the input. Valid if input signal type is normal digital input. |
|
0x3673–0x3676 |
13940–13943 |
R |
– |
DATETIME |
– |
– |
Timestamp for the last input change counter preset/reset Valid if input signal type is normal digital input. |
|
0x3677–0x3678 |
13944–13945 |
R |
– |
INT32U |
0–4294967294 |
– |
Number of pulses received Valid if input signal type is pulse digital input. |
|
0x3679–0x367C |
13946–13949 |
R |
– |
INT64 |
– |
– |
Resettable value of consumption Value = pulse weight x number of pulses received Valid if input signal type is pulse digital input. |
|
0x367D–0x3680 |
13950–13953 |
R |
– |
INT64 |
– |
– |
Accumulated non-resettable value of consumption Valid if input signal type is pulse digital input. |
|
0x3681–0x3684 |
13954–13957 |
R |
– |
DATETIME |
– |
– |
Timestamp of last resettable consumption value reset Valid if input signal type is pulse digital input. |
|
0x3685–0x3686 |
13958–13959 |
R |
W |
FLOAT32 |
– |
– |
Power calculation Valid if
|
|
0x3687–0x369E |
13960–13983 |
R |
– |
OCTET STRING |
– |
– |
Digital input identification coded over 45 ASCII characters(1) |
|
0x369F–0x36A0 |
13984–13985 |
R |
s |
FLOAT32 |
0.003–1 |
– |
Digital input 1 filter time |
|
0x36A1 |
13986 |
R |
– |
INT16U |
0–1 |
– |
Input contact type(1)
|
|
0x36A2 |
13987 |
R |
– |
INT16U |
0–1 |
– |
Input signal type(1)
|
|
0x36A3 |
13988 |
R |
– |
INT16U |
0–1 |
– |
Pulse polarity(1)
Valid if input signal type is pulse digital input. |
|
0x36A4 |
13989 |
R |
– |
INT16U |
1–4 |
– |
Pulse unit(1)
Valid if input signal type is pulse digital input. |
|
0x36A5–0x36A6 |
13990–13991 |
R |
– |
FLOAT32 |
1–16777215 |
– |
Pulse weight(1) (2) Valid if input signal type is pulse digital input. Factory setting = 1.0 |
|
0x36A7–0x36A8 |
13992–13993 |
R |
– |
INT32U |
1–4294967294 |
– |
Input counter threshold value(1) Valid if input signal type is normal digital input. Factory setting = 5000 |
|
0x36A9–0x36B8 |
13994–14009 |
– |
– |
– |
– |
– |
Reserved |
|
(1) Value set by using the EcoStruxure Power Commission software. (2) Examples:
|
|||||||