IFM Interface Identification
IFM Interface Firmware Revision
The IFM interface firmware revision starts at register 11776 and has a maximum length of eight registers.
The firmware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2DDF–0x2DEE |
11744–11759 |
R |
– |
OCTET STRING |
– |
Device family |
|
0x2DEF–0x2DF6 |
11760–11767 |
R |
– |
OCTET STRING |
– |
Product range |
|
0x2DF7–0x2DFE |
11768–11775 |
R |
– |
OCTET STRING |
– |
Product model |
|
0x2DFF–0x2E04 |
11776–11781 |
R |
– |
OCTET STRING |
– |
Firmware revision |
Serial Number for IFM Interface TRV00210 or STRV00210
The serial number of IFM interface TRV00210 or STRV00210 is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.
-
PP = plant code
-
YY = year of fabrication (05–99)
-
WW = week of fabrication (01–53)
-
D = day of fabrication (1–7)
-
nnnn = production number of the device on the day (0001–9999)
A read request of six registers is necessary to read the IFM interface serial number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E07 |
11784 |
R |
– |
OCTET STRING |
– |
‘PP’ |
|
0x2E08 |
11785 |
R |
– |
OCTET STRING |
‘05’–‘99’ |
‘YY’ |
|
0x2E09 |
11786 |
R |
– |
OCTET STRING |
‘01’–‘53’ |
‘WW’ |
|
0x2E0A |
11787 |
R |
– |
OCTET STRING |
D: ‘1’–‘7’ n: ‘0’–‘9’ |
‘Dn’ |
|
0x2E0B |
11788 |
R |
– |
OCTET STRING |
‘00’–‘99’ |
‘nn’ |
|
0x2E0C |
11789 |
R |
– |
OCTET STRING |
‘0’–‘9’ |
‘n’ (the NULL character ends the serial number) |
Serial Number for IFM Interface LV434000
The serial number of IFM interface LV434000 is composed of a maximum of 17 alphanumeric characters with the following format: PPPPPPYYWWDLnnnn0.
-
PPPPPP = plant code (example: BATAM plant code is 0000HL)
-
YY = year of fabrication (05–99)
-
WW = week of fabrication (01–53)
-
D = day of fabrication (1–7)
-
L = line or machine number (0-9 or a-z)
-
nnnn = production number of the device on the day (0001–9999)
A read request of ten registers is necessary to read the IFM interface serial number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E5C-0x2E5E |
11869-11871 |
R |
– |
OCTET STRING |
– |
‘PPPPPP’ |
|
0x2E5F |
11872 |
R |
– |
OCTET STRING |
‘05’–‘99’ |
‘YY’ |
|
0x2E60 |
11873 |
R |
– |
OCTET STRING |
‘01’–‘53’ |
‘WW’ |
|
0x2E61 |
11874 |
R |
– |
OCTET STRING |
D: ‘1’–‘7’ L: ‘0’–‘9’ or ‘a’–‘z |
‘DL’ |
|
0x2E62 |
11875 |
R |
– |
OCTET STRING |
‘00’–‘99’ |
‘nn’ |
|
0x2E63 |
11876 |
R |
– |
OCTET STRING |
‘00’–‘99’ |
‘nn’ |
|
0x2E64-0x2E65 |
11877-11878 |
R |
– |
OCTET STRING |
‘0’ |
‘0’ (the NULL character ends the serial number) |
Current Date and Time
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E73–0x2E76 |
11892–11895 |
R-WC |
– |
DATETIME |
– |
Current date and time in DATETIME format |
|
0x2E77–0x2E78 |
11896–11897 |
R |
Seconds |
INT32U |
0x00–0xFFFFFFFF |
Number of seconds counted since last start |
Product Identification
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E7C |
11901 |
R |
– |
INT16U |
– |
Product identification = 15146 for the IFM interface |
Hardware Revision for IFM Interface LV434000
The hardware revision of IFM interface LV434000 starts at register 11922 and has a maximum length of ten registers.
The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E91–0x2E96 |
11922–11927 |
R |
– |
OCTET STRING |
– |
Hardware revision |
Read Device Identification
The Read Device Identification function is used to access in a standardized manner the information required to identify a device clearly. The description is made up of a set of objects (ASCII character strings).
A complete description of the Read Device Identification function is available at www.modbus.org.
The coding for the identification of the IFM interface is the following:
|
Name |
Type |
Description |
|---|---|---|
|
Vendor name |
OCTET STRING |
‘Schneider Electric’ (18 characters) |
|
Product code |
OCTET STRING |
'LV434000’ or 'TRV00210' (1) or ‘STRV00210’ |
|
Firmware revision |
OCTET STRING |
‘XXX.YYY.ZZZ’ from IFM interface revision 002.002.000 |
|
Vendor URL |
OCTET STRING |
‘https://www.se.com’ (33 characters) |
|
Product name |
OCTET STRING |
‘ULP/Modbus-SL communication interface module’ |
|
(1) Product code returns ‘TRV00210-L’ when IFM interface TRV00210 is loaded with IFM legacy firmware. For more information, refer to MasterPact Modbus Legacy User Guide. |
||
IMU Identification
Identification of the IMU can be set by using the EcoStruxure Power Commission software. When not programmed, the IMU identification registers return 0 (0x0000).
The FDM121 display displays the first 14 characters of the IMU name.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2E18–0x2E2E |
11801–11823 |
R |
– |
OCTET STRING |
– |
IMU name = up to 45 ASCII characters ended by the NULL character 0x00 |
|
0x2E2F–0x2E38 |
11824–11833 |
R |
– |
OCTET STRING |
– |
Vendor name = ‘Schneider Electric’ |
|
0x2E39–0x2E42 |
11834–11843 |
R |
– |
OCTET STRING |
– |
Product Code = ‘TRV00210’ or ‘LV434000’ |
|
0x2E43–0x2E44 |
11844–11845 |
R |
– |
OCTET STRING |
– |
Reserved |
|
0x2E45–0x2E5B |
11846–11868 |
R |
– |
OCTET STRING |
– |
IMU location = up to 45 ASCII characters ended by the NULL character 0x00 |
@ Adrien > Confirm that 'LV434000' is returned for LV434000 with legacy firmware ??? Define the specificities of data and command for IFM legacy firmware ???