Time-Stamped Information
General Description
The time-stamped information enables the user to know all the dates related to important information.
The time-stamped information table describes:
-
the current date
-
the last current demand and corresponding dates
-
the last power demand and corresponding dates
-
the last reset and corresponding dates
-
the last k-factor demand peak and corresponding dates
-
the last current demand peak and corresponding dates
Current Date
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0BB7– 0x0BBA |
3000– 3003 |
R |
– |
– |
XDATE |
– |
P |
Current date of the metering manager |
|
0x2327– 0x232A |
9000– 9003 |
R |
– |
– |
XDATE |
– |
E/P |
Current date of the protection manager |
Last Current Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0BBC– 0x0BBE |
3005–3007 |
R |
– |
– |
DATE |
– |
E/P |
Date of last current demand maximum I1 (register 2204) |
|
0x0BBF– 0x0BC1 |
3008–3010 |
R |
– |
– |
DATE |
– |
E/P |
Date of last current demand maximum I2 (register 2205) |
|
0x0BC2– 0x0BC4 |
3011–3013 |
R |
– |
– |
DATE |
– |
E/P |
Date of last current demand maximum I3 (register 2206) |
|
0x0BC5– 0x0BC7 |
3014–3016 |
R |
– |
– |
DATE |
– |
E/P |
Date of last current demand maximum on the neutral (register 2207) (1) |
|
(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. |
||||||||
Last Power Demand
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0BC8– 0x0BCA |
3017– 3019 |
R |
– |
– |
DATE |
– |
E/P |
Date of last active power demand maximum (register 2224) |
|
0x0BCB– 0x0BCD |
3020– 3022 |
R |
– |
– |
DATE |
– |
P |
Date of last reactive power demand maximum (register 2230) |
|
0x0BCE– 0x0BD0 |
3023– 3025 |
R |
– |
– |
DATE |
– |
E/P |
Date of last apparent power demand maximum (register 2236) |
Last Reset
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0BD1– 0x0BD3 |
3026– 3028 |
R |
– |
– |
DATE |
– |
P |
Date of last reset of current demand maximum values |
|
0x0BD4– 0x0BD6 |
3029– 3031 |
R |
– |
– |
DATE |
– |
P |
Date of last reset of power demand maximum values |
|
0x0BD7– 0x0BD9 |
3032– 3034 |
R |
– |
– |
DATE |
– |
P |
Date-Time of last min. registers reset (1300–1599) (1) |
|
0x0BDA– 0x0BDC |
3035– 3037 |
R |
– |
– |
DATE |
– |
P |
Date-Time of last max. registers reset (1600–1899) (1) |
|
0x0BDD– 0x0BDF |
3038– 3040 |
R |
– |
– |
DATE |
– |
P |
Date of last reset of energy meters |
|
0x2331– 0x2333 |
9010– 9012 |
R |
– |
– |
DATE |
– |
P |
Date of last reset of the maximum phase, ground-fault, and earth-leakage currents |
|
0x236D– 0x236F |
9070– 9072 |
R |
– |
– |
DATE |
– |
P |
Date of last reset of the trip history (last 10 faults) |
|
0x2370– 0x2372 |
9073– 9075 |
R |
– |
– |
DATE |
– |
P |
Date of last reset of the alarm history (last 10 alarms) |
|
(1) This register is updated whenever any of the min. registers are reset. Command interface authorizes user to clear min. of current rms and unbalance values, voltage rms and unbal values, frequency, P/Q/S/PF, fundamental quantities and THD, voltage crest and current crest independently. However, since only one date/time of last reset is maintained, it is recommended to always set all bits in the command that resets min. values. |
||||||||
Last K-Factor Demand Peak
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0BE0– 0x0BE2 |
3041–3043 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last K-factor demand peak (phase 1) |
|
0x0BE3– 0x0BE5 |
3044–3046 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last K-factor demand peak (phase 2) |
|
0x0BE6– 0x0BE8 |
3047–3049 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last K-factor demand peak (phase 3) |
|
0x0BE9– 0x0BEB |
3050–3052 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last K-factor demand peak (Neutral) (1) |
|
(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. |
||||||||
Last Current Demand Peak
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0BEC– 0x0BEE |
3053– 3055 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last I2 demand peak (phase 1) |
|
0x0BEF– 0x0BF1 |
3056– 3058 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last I2 demand peak (phase 2) |
|
0x0BF2– 0x0BF4 |
3059– 3061 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last I2 demand peak (phase 3) |
|
0x0BF5– 0x0BF7 |
3062– 3064 |
R |
– |
– |
DATE |
– |
P |
Date of appearance of last I2 demand peak (Neutral) (1) |
|
(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. |
||||||||